Dear all,
I have built the fsl-image-gui by yocto, when booting it shows udev cannot setup, because my kernel doesn't support udev, so I add the "exit 0" at the top of /etc/iniit.d/udev,
then I can see the login part on terminal, but when I insert my usb mouse, it cannot work.
When inserting, log shows:
root@imx53qsb:/#
root@imx53qsb:/#
root@imx53qsb:/# usb 2-1.3: USB disconnect, address 4
usb 2-1.4: new low speed USB device using fsl-ehci and address 5
input: USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1.4:1.0/input/input8
generic-usb 0003:1BCF:0007.0003: input: USB HID v1.10 Mouse [USB Optical Mouse] on usb-fsl-ehci.1-1.4/input0
When I use the qt4e-demo-image, I can using my mouse for selecting each QT demo, but I cannot use it by fsl-image-gui.
Is there some command I forget to type in?
Thanks!
Zhang, this question can also be posted on the meta-freescale mailing list. So may get faster response for Yocto related issues.
Leo
Thanks!
is there any "startx" script in your filesystem?