Hi,iMX6ULZ
I am currently running Linux on iMX6ULZ SoC 4 x UART but I need one or two more UART, which iMX6 or iMX7 SoC I can select? I can use the NXP MFGTools to flash image to iMX6ULZ NAND, will the same tools compatible for all other iMX6 or iMX7 SoC?
Thank you.
Kind regards,
jhiMX6ULZ
Hi Jupiter
one can look at i.MX6 comparison table
https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for the response and the link, but there are more discrepancies between the two documents, in the document i.MX 6ULZ Applications Processors that the number of UART is 4 which I think is correct, where the FLYRIMXPRDCMPR.pdf that the number of UART is 8 which I think is wrong, could you please further clarify it?
Thank you.
Kind regards.