Hello Community,
We are in the process of moving from the LTIB build system to a Yocto one and have noticed missing UARTs on the iMX6DL. (We are using a Congatec qmx6 PN16111 and code from their git repository)
On the old LTIB build, the kernel detects 3 UARTS:
---------------------------------------------------------------------------------------------------------
[ 2.212509] imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
[ 2.268576] console [ttymxc1] enabled, bootconsole disabled
[ 2.268576] console [ttymxc1] enabled, bootconsole disabled
[ 2.280442] imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
[ 2.287378] imx-uart.4: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
[ 2.302894] brd: module loaded
...
root@linaro:/sys/class/tty# ls -las ttymx*
0 lrwxrwxrwx 1 root root 0 2014-09-30 02:23 ttymxc1 -> ../../devices/platform/imx-uart.1/tty/ttymxc1
0 lrwxrwxrwx 1 root root 0 2014-09-30 02:23 ttymxc2 -> ../../devices/platform/imx-uart.2/tty/ttymxc2
0 lrwxrwxrwx 1 root root 0 2014-09-30 02:23 ttymxc4 -> ../../devices/platform/imx-uart.4/tty/ttymxc4
---------------------------------------------------------------------------------------------------------
But on the newer Yocto 1.6 build, there is only 1 and the class path is different.
---------------------------------------------------------------------------------------------------------
VGEN6: 1800 mV
Serial: IMX driver
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
console [ttymxc1] enabled
serial: Freescale lpuart driver
...
root@cgtqmx6:/sys/class/tty# ls -las
0 lrwxrwxrwx 1 root root 0 Sep 30 02:25 ttymxc1 -> ../../devices/soc0/soc.1/2100000.aips-bus/21e8000.serial/tty/ttymxc1
---------------------------------------------------------------------------------------------------------
From what I can tell (and I am no means an expert) the newer build extracts the machine info from the dtb file, while in the older build it can't find a dtb file. The dtb file contains all the UART information, but for some reason, the kernel just doesn't see the other UARTs. Am I missing a configuration setting somewhere else? Do I need something in uboot?
Thanks in advance.
解決済! 解決策の投稿を見る。
Thank you very much for pointing out this insufficiency of our conga-QMX6 kernel implementation. We appreciate your suggestions very much.
In order to fix the problem, we've created a patch that can be found in our kernel repository:
https://git.congatec.com/arm/qmx6_kernel/commit/9a3e94917d94b901b674cece0a3576b427a63b12
best regards,
Michael Schanz
If the dts has all the 3 uart nodes then all the three should be probed. Are you sure all the three nodes are present in the dts for your board?
Hi Fabio,
The dtb it is searching for is imx6dl-qmx6.dtb. Inside imx6dl-qmx6.dts there is #include "imx6dl.dtsi", which has the following:
uart1: serial@02020000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x02020000 0x4000>;
interrupts = <0 26 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 25 4 0>, <&sdma 26 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart2: serial@021e8000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021e8000 0x4000>;
interrupts = <0 27 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 27 4 0>, <&sdma 28 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart3: serial@021ec000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021ec000 0x4000>;
interrupts = <0 28 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 29 4 0>, <&sdma 30 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart4: serial@021f0000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021f0000 0x4000>;
interrupts = <0 29 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 31 4 0>, <&sdma 32 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
...
I can see the status as "disabled" for all the UARTS, but how does /dev/ttymxc1 appear and the console work? Do the bootargs from uboot enable ttymxc1? FYI, my cmdline value has "console=ttymxc1,115200"
No, you need to really look at imx6dl-qmx6.dts. It is there that you need to activate the uarts you want via 'status=okay' andl also by providing the IOMUX configuration for the uarts.
imx6dl.dtsi has all the uarts defined and disabled, because this is a description of the SoC.
It is in your board dts that you specify what are the UART ports that are available in that particular hardware.
Actually you need to look at imx6qdl-qmx6.dtsi:
There is only one uart enabled in this dtsi, so the current behaviour is expected.
You should enable the other uarts in this file.
Thank you very much for pointing out this insufficiency of our conga-QMX6 kernel implementation. We appreciate your suggestions very much.
In order to fix the problem, we've created a patch that can be found in our kernel repository:
https://git.congatec.com/arm/qmx6_kernel/commit/9a3e94917d94b901b674cece0a3576b427a63b12
best regards,
Michael Schanz
Thank you Michael and Fabio, the patch works.
VGEN6: 1800 mV
Serial: IMX driver
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
console [ttymxc1] enabled
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
serial: Freescale lpuart driver
[drm] Initialized drm 1.1.0 20060810
root@cgtqmx6:/sys/class/tty# ls -las ttymxc*
0 lrwxrwxrwx 1 root root 0 Jan 1 1970 ttymxc1 -> ../../devices/soc0/soc.1/2100000.aips-bus/21e8000.serial/tty/ttymxc1
0 lrwxrwxrwx 1 root root 0 Jan 1 1970 ttymxc2 -> ../../devices/soc0/soc.1/2100000.aips-bus/21ec000.serial/tty/ttymxc2
0 lrwxrwxrwx 1 root root 0 Jan 1 1970 ttymxc4 -> ../../devices/soc0/soc.1/2100000.aips-bus/21f4000.serial/tty/ttymxc4
root@cgtqmx6:/sys/class/tty# uname -a
Linux cgtqmx6 3.10.17-1.0.0_qmx6+g4138f5b #1 SMP PREEMPT Wed Oct 8 07:53:08 EST 2014 armv7l GNU/Linux
root@cgtqmx6:/sys/class/tty#
Hi All,
Could any one tell me how to open ttymxc* ?
i can see below things.
$ ls -las /dev/ttymx*
0 crw------- 1 root tty 207, 16 Feb 23 15:39 /dev/ttymxc0
0 crw------- 1 root root 207, 20 Jan 1 1970 /dev/ttymxc4
0 crw------- 1 root root 207, 21 Jan 1 1970 /dev/ttymxc5
Chandini
Excellent, Michael.
I have also seen Alex de Cabo's patch updating Yocto to include such patch.
Also, if you have a chance it would be nice to have congatec support in the mainline kernel.
Thanks,
Fabio Estevam