Minimum external DDR3 amount

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Minimum external DDR3 amount

914 次查看
olli_mannisto
Contributor II

The i.MX7Solo datasheet says the DDR interface density is 256MB to 2GB (9.1.2 table 9-1). Does that actually mean that using 512Mbit or 1Gbit DDR3 chips is out of the question?

标签 (1)
0 项奖励
回复
2 回复数

828 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX7 DDRC supports devices with column size of 8-12 bits and row size of 11-16 bits;

data port size 16/32-bit; up to two CSs. Total memory size is restricted by 2048 MBytes (look at system

memory map).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

828 次查看
olli_mannisto
Contributor II

Hei, 

I was asking about minimum memory size. Are we fine with 512Mbit (32MBx16) part that's organized 12bit Row, 10bit Column? Apparently yes, but the datasheet claims 256MB is the minimum RAM size? 

0 项奖励
回复