I'm using i.mx6 processor. I have few doubts related to mfg tool by freescale.
MFG Tool is used to download OS images into target. But is it possible to
load executable code in .bin or .hex format into target using MFG Tool ?
解決済! 解決策の投稿を見る。
Hi Avadhut,
MFG tool can be used to download bin image to target board. You can download imx6_platform_sdk_v1.1.0.tgz from freescale.com.
It includes the document which has the detailed explanation about how to build binary and download binary file with mfg tool or load elf file with JTAG.
i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license.
Grace
Thank you raymond...
Thank you Grace and Raymond for reply... One more doubt i had about mfg tool... Is it that only USB OTG interface is required on target board to use mfg tool and other interfaces won't work ?
According to all what I know currently, only usb otg port is supported.
I think you'd better to read MFG tool documents especially <Manufacturing Tool V2 UTP Introduction.docx>. That can help you to understanding
MFG working theory.
Hi Avadhut,
MFG tool can be used to download bin image to target board. You can download imx6_platform_sdk_v1.1.0.tgz from freescale.com.
It includes the document which has the detailed explanation about how to build binary and download binary file with mfg tool or load elf file with JTAG.
i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license.
Grace