Dear community members,
I reviewed 32-bit DDR Interface using I.MX6 Dual Core but don't decide to use SDRAM_SDCLK0 or SDRAM_SDCLK1 for 32-bit mode.
According to EVM, DRAM_SDCLK_1 was applied to DDR3_D[0:31] ICs , I didn't understood exactly why SDRAM_SDCLK1 was applied to DDR3_D[0:31] ICs instead of SDRAM_SDCLK0.
Q1) If I use DRAM_SDCLK_0 instead of SDRAM_SDCLK1 for 32-bit mode DDR3 ( 2 * ICs) , Is there no problem?
Q2) If I use DRAM_SDCLK_1 for 32-BIT mode DDR3 Interface, Is there no problem?
Could you advice questions for me?
Thank
Solved! Go to Solution.
DRAM clock signals SDCLK0 and SDCLK1 are the practically the same (by default) and in this sense do no relate to CS0 or CS1
channels.
DRAM clock signals SDCLK0 and SDCLK1 are the practically the same (by default) and in this sense do no relate to CS0 or CS1
channels.