Hello, I'm using MX8M Mini EVK with Android 9, under Windows 10. *ADB works* fine but I have a real trouble getting into fastboot mode. I researched hard in all NXP documents - "Android_User's_Guide.pdf", "Android_Quick_Start_Guide.pdf" and even followed iMX6 instructions on how to config fastboot. Nothing works though.
1. Obviously, both "developer mode" as well as "OEM unlocked" option are enabled.
2. When I run "adb shell reboot bootloader" the board is being rebooted but all I see is a blanked screen and both "fastboot oem unlocked" nor "fastboot usb" command ever returns.
3. I have the latest Google USB driver installed (tried to add vendor ID from iMX6 documentations, didn't really work either)
4. It should be noted that I was able to flush the images through UUU (with a new NXP build android_p9.0.0_2.0.0-ga_image_8mmevk.tar.gz) but even with this new build the board won't enter fastboot mode.
Is there any change that needs to take place in the "android_winusb.inf" or "adb_usb.ini" ?
One last note, once the EVK board is booted in attempt to get into fastboot, instead of seeing "EVK_8MM" the device is changed to "USB download gadget", no idea if that's normal?
I will appreciate any help!
Thanks, Mike
解決済! 解決策の投稿を見る。
Hello,
This may be due to the host PC selects an incorrect driver model of the USB devices, leading to the PC inability to find fastboot device.
After accessing fastboot, run "reboot bootloader" in console after boot, in host side open "Computer Management->Device Manager", you'll note that the USB appears as:
Universal Serial Bus devices -> USB download gadget,
Right click it, and choose “Updated Driver -> browse my computer for driver software ->
let me pick from a list of available drivers on my computer”, clear “Show compatible hardware” item, then choose “ADB devices”,
Select yes to the pop-up window, this will select the USB as an ADB device,
This should fix the issue, and the fastboot device should be listed.
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Qu'est-ce que le pilote du gadget fastboot ?
Le pilote de gadget fastboot est un petit programme logiciel qui permet de démarrer des appareils tels que des smartphones et des tablettes à partir d'un ordinateur en utilisant le protocole fastboot.spd fastboot driver
Fastboot est un outil de ligne de commande de bas niveau utilisé dans le développement Android. Il peut être utilisé pour démarrer un appareil Android en mode de récupération, écrire des fichiers sur l'appareil ou monter et accéder au stockage de données de l'appareil.
Hi
I have this problem too on Windows 10 and I followed the guide to solve the problem. However the device manager keeps showing "USB download gadget" after installing the Google Driver from https://dl.google.com/android/repository/usb_driver_r13-windows.zip
I would expect something else?
I did try on a MAC with newly Android Studio installed and here fastboot gets instant contact to the device.
Ideas to overcome this?
Best regards
Svend
Hi Shivani,
Your solution is working only on connected device. If new device is connected and switched to fastboot mode. device couldn't be found. Then we have to select adb device manually again. This works for one device. But this has big productivity issue in factory. Can you help to solve this?
Hi, taesub_youn@whirlpool.com
Please update the USB Driver from this link to resolve this issue.
Regards,
Shivani
HI @shivanipatel ,
I have Apalis imx8qm som, with custom board. Fastboot is working with ubuntu system but not for windows 10 system, I have downloaded the files from this link, but still in device manager showing the connect usb as "USB download gadget".
After doing
Right click it, and choose “Updated Driver -> browse my computer for driver software ->
let me pick from a list of available drivers on my computer”, clear “Show compatible hardware” item, then choose “ADB devices” step, The usb driver still showing the "USB download gadget", and not coming in fastboot (not showing list of fastboot devices).
Kindly provide a solution.
Hello,
Greetings of the day!
Any update on this?
Hi Shivani,
This is for the same request that was queried by Taesub Youn earlier.
"Your solution is working only on connected device. If new device is connected and switched to fastboot mode. device couldn't be found. Then we have to select adb device manually again. This works for one device. But this has big productivity issue in factory. Can you help to solve this?"
I tried the solution that you had suggested. Installed the Google USB driver (from this link) through the Android SDK manager/tools.
However, it seems like the first time the device is connected, it still does not show up in fastboot mode. We have to manually update the driver from WinUsb devices to adb devices (Device manager -> update driver -> USB download gadget -> adb devices).
Once we update the driver manually, the `fastboot devices` command works,
However, all other fastboot commands fails as below
After the driver was manually updated, once we power cycle the device, then all the fastboot commands are working.
Is there an automatic way to update the driver so that each new device when connected to the PC for the first time gets recognized in the fastboot mode without manually updating the driver (and without rebooting the device)?
Thanks,
Regards,
Anupama
Hi, mike malgin
Please use the latest fastboot binaries from this link (for windows and linux) and follow the steps mentioned by Aldo Gutierrez to select the proper driver, you will be able to find the device in fastboot mode.
Let us know if you are still facing the issue.
Regards,
Shivani
Hello,
This may be due to the host PC selects an incorrect driver model of the USB devices, leading to the PC inability to find fastboot device.
After accessing fastboot, run "reboot bootloader" in console after boot, in host side open "Computer Management->Device Manager", you'll note that the USB appears as:
Universal Serial Bus devices -> USB download gadget,
Right click it, and choose “Updated Driver -> browse my computer for driver software ->
let me pick from a list of available drivers on my computer”, clear “Show compatible hardware” item, then choose “ADB devices”,
Select yes to the pop-up window, this will select the USB as an ADB device,
This should fix the issue, and the fastboot device should be listed.
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Aldo,
We noticed that USB ID getting changed on every build (EVT, DVT, etc). This is causing us to reconfigure windows machines at every build, impacting productivity. What is the reason behind the change? So far we have seen following IDs.
ID 18d1:4ee7 Google Inc.
ID 0525:a4a5 Netchip Technology, Inc. Pocketbook Pro 903
ID 03f0:0667 HP, Inc
-Pad