MMPF0100 rise time of regulators for start-up.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 rise time of regulators for start-up.

ソリューションへジャンプ
780件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about MMPF0100.

Please see Figure 6 and Table 11 of MMPF0100 datasheet (Rev.15), tr3 is difined as 0.2ms.

Our customer want to know whether the rise time by SWxDVSSPEED setting.

I feel SWxDVSSPEED changes the slew rate for DVS only, and no effect for rise time when start-up, so the rise time (0.2ms) cannot be changed.

Is my understanding correct?

Or SWxDVSSPEED changes the start-up rise time?

Best Regards,

Satoshi Shimoda

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
622件の閲覧回数
art
NXP Employee
NXP Employee

You are right in that the SWxDVSSPEED settings only affect the DVS operation and do not affect the power-on voltage rise time that is fixed and its typical value is 0.2ms.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
623件の閲覧回数
art
NXP Employee
NXP Employee

You are right in that the SWxDVSSPEED settings only affect the DVS operation and do not affect the power-on voltage rise time that is fixed and its typical value is 0.2ms.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信