MIMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1064

1,264件の閲覧回数
StarMao159376
Contributor II

Does mimxrt1064 support local bus?

0 件の賞賛
返信
1 返信

1,257件の閲覧回数
Yuri
NXP Employee
NXP Employee

@StarMao159376 
Hello,

   If I understand the question correctly, the i.MX RT does not support a local bus
(internal bus, common for all i.MX RT internal modules)  for external devices. 
  The most close for customer's purposes - I think - is the SEMC (Smart External Memory
Controller).
     "The SEMC is a multi-standard memory controller optimized for both high-performance
and low pin-count. It can support multiple external memories in the same
application with shared address and data pins. The interface supported includes SDRAM,
NOR Flash, SRAM, and NAND Flash, as well as 8080 display interface."

Regards,
Yuri.

0 件の賞賛
返信