MFGTool烧写问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGTool烧写问题

5,071 Views
yinkai
Contributor II

IMX6DL的板子,使用MFGTool烧写过程中出现错误,Boot" body="BootStrap" error, file="C:\Users\elker\Desktop\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\u-boot.bin,之前板子是可以正常烧写的,出现这种现象是是USB_OTG问题还是DDR问题,谢谢

pastedImage_0.png

Labels (1)
0 Kudos
Reply
6 Replies

2,665 Views
jian_jiang
NXP Employee
NXP Employee

Hi yin kai,

Maybe the connection of usb cable is not very stable, and you can change another.

Pls make sure you choose the correct mfgtools script for IMX6DL first.

All the best

Kane Jiang

0 Kudos
Reply

2,665 Views
aravinthkumarja
Senior Contributor II

Hi yinkai​,

Can you attach MFGTool.log file, then only we found the error.

Regards,

Aravinth

0 Kudos
Reply

2,665 Views
yinkai
Contributor II

hello,log as follow:

DLL version: 2.2.3

Monday, June 27, 2016 10:20:52   Start new logging

ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[003C07E0]

ModuleID[2] LevelID[10]: Device Manager thread is running

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\Users\elker\Desktop\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\u-boot.imx

ModuleID[2] LevelID[1]: MxHidDevice::Write() Error writing to device 0x57.

ModuleID[2] LevelID[1]: Failed to initialize memory!

ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Boot excute failed

ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\Users\elker\Desktop\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\u-boot.imx

ModuleID[2] LevelID[1]: MxHidDevice::Write() Error writing to device 0x57.

ModuleID[2] LevelID[1]: Failed to initialize memory!

ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Boot excute failed

ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed

ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed

ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - EVENT_KILL

ModuleID[2] LevelID[10]: CMyExceptionHandler::OnMsgExceptionEvent() - KillExceptionHandlerThread

ModuleID[2] LevelID[10]: Exception Handler thread is closed

ModuleID[2] LevelID[1]: delete MxHidDeviceClass

ModuleID[2] LevelID[10]: delete MxHidDevice[003C07E0]

ModuleID[2] LevelID[10]: Device Manager thread is closed

0 Kudos
Reply

2,665 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi yin kai,

Which version BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,665 Views
yinkai
Contributor II

FSL Community BSP中的

2.0 - codename Jethro

0 Kudos
Reply

2,665 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi yin kai,

Here I can not know which version BSP are you using, so I just guess the failed downloading maybe caused by the non-matched version mfgtool. It means the Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER version mfgtool can not work for your BSP. Here recommend you to download the bsp, demo images and documents from our webstie. The llink is i.MX 6 Series Software and Development Tool|NXP . Hope this can help you. Any questions you can contact me easily.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply