https://github.com/nxp-mcuxpresso/mcux-sdk-examples/blob/main/evkmimx8mp/driver_examples/rdc/
IMX8MP evaluation board | SCH-46370 REV B1 |
Affected BSP | All BSPs from NXP website with kernel lf-5.10.y and lf-5.15.y |
MCUXpresso SDK version | SDK_2.13.0_EVK-MIMX8MP |
Testing Procedure:
Case 1, in U-Boot:
load mmc 2:2 0x70000000 lib/firmware/rdc.bin cp.b 70000000 0x7e0000 20000 bootaux 0x7e0000
Case 2, in Linux:
echo -n rdc.elf > /sys/class/remoteproc/remoteproc0/firmware echo start > /sys/class/remoteproc/remoteproc0/state
Expected Output:
RDC Example: RDC Peripheral access control RDC Peripheral access control with SEMA42 RDC memory region access control RDC Example Success
Actual Output (in both cases):
RDC Example: RDC Peripheral access control
I also tried running each of the three test cases APP_RDC_Periph(), APP_RDC_PeriphWithSema42() and APP_RDC_Mem() by commenting out the other two, all failed. Even though HardFault_Handler was triggered, memDemoError equals 3 in Fault_Handler.
However, the same RDC example for IMX8MM evk works perfectly:
https://github.com/nxp-mcuxpresso/mcux-sdk-examples/tree/main/evkmimx8mm/driver_examples/rdc
IMX8MM evaluation board | SCH-31407 REV C4 |
Tested BSP | All BSPs from NXP website with kernel lf-5.10.y and lf-5.15.y |
MCUXpresso SDK version | SDK_2.13.0_EVK-MIMX8MM |
Any help or suggestion is much appreciated!
Thank you for contacting NXP support!
This application can't support running with Uboot! and accordingly, it does not support Flash target and DDR target!
This example aims to show the basic usage of the IP's function, some of the used Resources are assigned to the Cortex-A core by uboot.
mcux-sdk-examples/readme.txt at main · nxp-mcuxpresso/mcux-sdk-examples (github.com)
Thanks for the prompt help, Chavira.
This application can't support running with Uboot!
As I mentioned, I also tried running it by remoteproc in Linux.
accordingly, it does not support Flash target and DDR target!
OK. But the application is compiled with MIMX8ML8xxxxx_cm7_ram.ld rather than MIMX8ML8xxxxx_cm7_ddr_ram.ld nor MIMX8ML8xxxxx_cm7_flash.ld. It should have supported running from TCM.
some of the used Resources are assigned to the Cortex-A core by uboot
I believe you were referring to this RDC configuration assigned by SPL. I have removed them and loaded the new UBoot, the example still doesn't work.
Could you please suggest what else I can try?