MC33PF8100EPES for i.MX8QM issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33PF8100EPES for i.MX8QM issues

1,365 Views
Sam1978
Contributor II

i setup 2 MC33PF8100 chipset on PCB borad for Power suplier,i want communication to 8100EPES with I2C bus for cpu core voltage ,but can not program via i2c bus to imply voltage adjustment,pls contact me if someone knew what problem was,thanks

 

0 Kudos
Reply
3 Replies

1,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sam

 

examples of i2c communication with pmic can be found in SCFW sources:  ..mx8qm_mek /board.c

SCFW Porting Kit​ 1.8.0

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

also may be useful AN12631  Normal and Secure Debug for i.MX8/8X Family of Applications Processors

 

Best regards
igor

0 Kudos
Reply

1,337 Views
Sam1978
Contributor II

Hi guy:

 Can you tell me what steps i need follow? i just want to program MC33PF8100EPES(2 chipsets),i found some USB 2 I2C software, try to read or write these to chipsets,but i failed ,data read from chipset was not correct,write access denied,send me it if you have a software that adequate operation

 what i need do if i read or write these 2 MC33PF8100EPES chipsets,such as adjust level for VDDOTP and TBBEN ,Poweron IO?

 the Register groups are functions regester,OTP mirror register,OTP config for hardwire

 

 thanks

Sam

 

Tags (1)
0 Kudos
Reply