I am using the kernel on branch imx_5.4.47_2.2.0 from https://source.codeaurora.org/external/imx/linux-imx.git for a iMX6ULL SOC.
Yet there is no driver for the PF1550 PMIC ?
Searching the internet some kernel patches can be found.
Yet I wonder if there is some "official" driver for this FSL PMIC ?
Thanks Thomas
解決済! 解決策の投稿を見る。
Hi thomasritter ,
There is no pf1550 driver in L5.4.x BSP, but it's driver is supported in L4.19.35_1.1.0 : drivers/regulator/pf1550.c
and it is supported in device tree for i.MX6UL: arch/arm/boot/dts/imx6ul-14x14-evk-pf1550.dts
so you can port it to L5.4.x BSP.
Hope this information is helpful to you.
Have a nice day!
B.R,
Weidong
Hi thomasritter ,
There is no pf1550 driver in L5.4.x BSP, but it's driver is supported in L4.19.35_1.1.0 : drivers/regulator/pf1550.c
and it is supported in device tree for i.MX6UL: arch/arm/boot/dts/imx6ul-14x14-evk-pf1550.dts
so you can port it to L5.4.x BSP.
Hope this information is helpful to you.
Have a nice day!
B.R,
Weidong