Looking for PMIX PF1550 mfd kernel driver (imx_5.4.47_2.2.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for PMIX PF1550 mfd kernel driver (imx_5.4.47_2.2.0)

Jump to solution
1,019 Views
thomasritter
Contributor I

I am using the kernel on branch imx_5.4.47_2.2.0 from https://source.codeaurora.org/external/imx/linux-imx.git for a iMX6ULL SOC.

Yet there is no driver for the PF1550 PMIC ?

Searching the internet some kernel patches can be found.

Yet I wonder if there is some "official" driver for this FSL PMIC ?

Thanks Thomas

Labels (2)
0 Kudos
Reply
1 Solution
1,013 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi thomasritter ,

    There is no pf1550 driver in L5.4.x BSP, but it's driver is supported in L4.19.35_1.1.0 : drivers/regulator/pf1550.c

     and it is supported in device tree for i.MX6UL: arch/arm/boot/dts/imx6ul-14x14-evk-pf1550.dts

     so you can port it to L5.4.x BSP.

Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong

View solution in original post

0 Kudos
Reply
1 Reply
1,014 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi thomasritter ,

    There is no pf1550 driver in L5.4.x BSP, but it's driver is supported in L4.19.35_1.1.0 : drivers/regulator/pf1550.c

     and it is supported in device tree for i.MX6UL: arch/arm/boot/dts/imx6ul-14x14-evk-pf1550.dts

     so you can port it to L5.4.x BSP.

Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply