Hello,
I need to configure the flexcan in imx6 for mail box reception and transmission(I want to use complete 64 mailboxes). But the current driver support only FIFO reception(Linux kernel 3.0.35). From where can i get the driver for mailbox? or can we need to write the code from scratch?. Please give some replay or send me the useful links/codes because i need to complete this task with in a short period...
Regards
Shabeer
已解决! 转到解答。
Hi Sorry for the late replay...
We implemented the mailbox reception logic in flexcan driver.
Regards
Shabeer
Hi,
I forgot to say my complete requirement.. I want to use both FIFO and mailbox mechanisms. That is the first 8 message boxes are used for FIFO reception(current flexcan driver support it ) and the remaining message boxes are used for mailbox reception and transmission..Please give ur valuable replay..
Thanks and Regards,
Shabeer
Shabeer
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Hello,
I know this post is old, but I wander how do you code the mailbox reception. I am trying to do the same thing using socketcan but i don't know if i have to use a completly different system (like sysfs) to access the Mailbox buffer or if it's better to modify directly the socketcan lib to access it.
Thanx for your reply.