You don't need set IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT alone, it was covered in MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC, when the BSP initializing the PIN EIM_DA12 as CSI1_VSYNC, the IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT will be set too.
From the define, we can know the IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT register will be set to 0x1.
/*
* The pin function ID is a tuple of
* <mux_reg conf_reg input_reg mux_mode input_val>
*/
#define MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x144 0x458 0x8e4 0x2 0x1
the Linux BSP documentation may useful for you. You can download it from here:
< http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW >
Under Documentation -- >
For reference, please read the i.MX_6Dual6Quad_BSP_Porting_Guide.pdf and i.MX_6Dual6Quad_Linux_Reference_Manual.pdf .
Hi,
I am facing some problem while receiving RGB Bayer video data from 12-bit (parallel) aptina sensor.
In summary, the application times-out while DQ operation:
In MVC:mxc_v4l_dqueue
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
When I probe the lines from the sensor, I am able to see activity on the HSYNC, VSYNC, PIXCLK and DATA.
Setup details:
Out of 12 data lines, 2 lines are not connected, effectively making it a 10-bit interface.
The LOG while running the 'yavta' application is as below: ./yavta -i 1 -f SBGGR10 -c=10 -s 1280x720 -n 2 /dev/video0
********************************************************************
In MVC: mxc_v4l_open
device name is Mxc Camera
End of mxc_v4l_open: v2f pix widthxheight 1280 x 720
End of mxc_v4l_open: crop_bounds widthxheight 1280 x 720
End of mxc_v4l_open: crop_defrect widthxheight 1280 x 720
End of mxc_v4l_open: crop_current widthxheight 1280 x 720
On Open: Input to ipu size is 1280 x 720
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 80685600
case VIDIOC_QUERYCAP
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0045627
case VIDIOC_S_INPUT
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 80045626
case VIDIOC_G_INPUT
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0cc5605
case VIDIOC_S_FMT
- In MVC: mxc_v4l2_s_fmt
type=V4L2_BUF_TYPE_VIDEO_CAPTURE
End of mxc_v4l2_s_fmt: v2f pix widthxheight 1280 x 720
End of mxc_v4l2_s_fmt: crop_bounds widthxheight 1280 x 720
End of mxc_v4l2_s_fmt: crop_defrect widthxheight 1280 x 720
End of mxc_v4l2_s_fmt: crop_current widthxheight 1280 x 720
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0cc5604
case VIDIOC_G_FMT
In MVC: mxc_v4l2_g_fmt type=1
type is V4L2_BUF_TYPE_VIDEO_CAPTURE
End of mxc_v4l2_g_fmt: v2f pix widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_bounds widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_defrect widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_current widthxheight 1280 x 720
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0145608
case VIDIOC_REQBUFS
In MVC:mxc_streamoff
MVC: In mxc_free_frame_buf
In MVC:mxc_allocate_frame_buf - size=1843200
cma: dma_alloc_from_contiguous(cma dc0e4ec0, count 450, align 8)
cma: dma_alloc_from_contiguous(): returned 81cd2000
cma: dma_alloc_from_contiguous(cma dc0e4ec0, count 450, align 8)
cma: dma_alloc_from_contiguous(): returned 81cd6000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x76400, start=0x76cd2000, end=0x76e94000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x76600, start=0x76b10000, end=0x76cd2000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 40045612
case VIDIOC_STREAMON
In MVC:mxc_streamon
IPU:In csi_enc_enabling_tasks
cma: dma_alloc_from_contiguous(cma dc0e4ec0, count 450, align 8)
cma: dma_alloc_from_contiguous(): returned 81cda000
In csi_enc_setup
imx-ipuv3 2800000.ipu: init channel = 15
imx-ipuv3 2800000.ipu: ipu busfreq high requst.
imx-ipuv3 2800000.ipu: IPU_CONF = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CONF = 0x0000002F
imx-ipuv3 2800000.ipu: IDMAC_CHA_EN1 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CHA_EN2 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI1 = 0x18800001
imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI2 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_BAND_EN1 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_BAND_EN2 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL0 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL0 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL1 = 0x00000000
imx-ipuv3 2800000.ipu: DMFC_WR_CHAN = 0x00000090
imx-ipuv3 2800000.ipu: DMFC_WR_CHAN_DEF = 0x202020F6
imx-ipuv3 2800000.ipu: DMFC_DP_CHAN = 0x00009694
imx-ipuv3 2800000.ipu: DMFC_DP_CHAN_DEF = 0x2020F6F6
imx-ipuv3 2800000.ipu: DMFC_IC_CTRL = 0x00000002
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW2 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW3 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_DISP_FLOW1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_FSIZE = 0x00000000
imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_C = 0x00000000
imx-ipuv3 2800000.ipu: IPU_IC_CONF = 0x40000000
setting IDMAC channel parameters for GENERIC-16 mode
imx-ipuv3 2800000.ipu: initializing idma ch 0 @ f0180000
!!! : setting RWS enable for generic sensor
imx-ipuv3 2800000.ipu: IPU_CONF = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CONF = 0x0000002F
imx-ipuv3 2800000.ipu: IDMAC_CHA_EN1 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CHA_EN2 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI1 = 0x18800001
imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI2 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_BAND_EN1 = 0x00000000
imx-ipuv3 2800000.ipu: IDMAC_BAND_EN2 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL0 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL0 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL1 = 0x00000000
imx-ipuv3 2800000.ipu: DMFC_WR_CHAN = 0x00000090
imx-ipuv3 2800000.ipu: DMFC_WR_CHAN_DEF = 0x202020F6
imx-ipuv3 2800000.ipu: DMFC_DP_CHAN = 0x00009694
imx-ipuv3 2800000.ipu: DMFC_DP_CHAN_DEF = 0x2020F6F6
imx-ipuv3 2800000.ipu: DMFC_IC_CTRL = 0x00000002
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW2 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW3 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_FS_DISP_FLOW1 = 0x00000000
imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_FSIZE = 0x00000000
imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_C = 0x00000000
imx-ipuv3 2800000.ipu: IPU_IC_CONF = 0x40000000
imx-ipuv3 2800000.ipu: ch 0 word 0 - 00000000 00000000 00000000 E0001800 000B3C9F
imx-ipuv3 2800000.ipu: ch 0 word 1 - 0ED00000 01DA0000 00C7C000 00027FC0 00000000
imx-ipuv3 2800000.ipu: PFS 0x6,
imx-ipuv3 2800000.ipu: BPP 0x3,
imx-ipuv3 2800000.ipu: NPB 0x1f
imx-ipuv3 2800000.ipu: FW 1279,
imx-ipuv3 2800000.ipu: FH 719,
imx-ipuv3 2800000.ipu: EOL1 0,
imx-ipuv3 2800000.ipu: EBA0 0x76800000
imx-ipuv3 2800000.ipu: EBA1 0x76800000
imx-ipuv3 2800000.ipu: Stride 2559
imx-ipuv3 2800000.ipu: scan_order 0
imx-ipuv3 2800000.ipu: uv_stride 0
imx-ipuv3 2800000.ipu: u_offset 0x0
imx-ipuv3 2800000.ipu: v_offset 0x0
imx-ipuv3 2800000.ipu: Width0 0+1,
imx-ipuv3 2800000.ipu: Width1 0+1,
imx-ipuv3 2800000.ipu: Width2 0+1,
imx-ipuv3 2800000.ipu: Width3 0+1,
imx-ipuv3 2800000.ipu: Offset0 0,
imx-ipuv3 2800000.ipu: Offset1 0,
imx-ipuv3 2800000.ipu: Offset2 0,
imx-ipuv3 2800000.ipu: Offset3 0
eba 76400000
eba 76600000
IPU_CONF 0x00000102
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445611
case VIDIOC_DQBUF
In MVC:mxc_v4l_dqueue
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0145608
case VIDIOC_REQBUFS
In MVC:mxc_streamoff
imx-ipuv3 2800000.ipu: CSI stop timeout - 5 * 10ms
imx-ipuv3 2800000.ipu: ipu busfreq high release.
cma: dma_release_from_contiguous(page 81cda000)
In MVC:mxc_free_frames
MVC: In mxc_free_frame_buf
cma: dma_release_from_contiguous(page 81cd2000)
cma: dma_release_from_contiguous(page 81cd6000)
In MVC:mxc_allocate_frame_buf - size=1843200
In MVC:mxc_v4l_close
In MVC:mxc_streamoff
mxc_v4l_close: release resource
MVC: In mxc_free_frame_buf
In MVC:mxc_free_frames
power_down_callback
********************************************************************
I have added the required support for bayer in the sources as per the discussion:
https://community.freescale.com/message/353698?et=watches.email.thread#353698
The sensor is connected to CSI1-IPU2.
My DTS has the following configuration:
ipu2: ipu@02800000 {
compatible = "fsl,imx6q-ipu";
reg = <0x02800000 0x400000>;
interrupts = <0 8 0x4 0 7 0x4>;
clocks = <&clks 133>, <&clks 134>, <&clks 137>,
<&clks 41>, <&clks 42>,
<&clks 135>, <&clks 136>;
clock-names = "bus", "di0", "di1",
"di0_sel", "di1_sel",
"ldb_di0", "ldb_di1";
resets = <&src 4>;
bypass_reset = <0>;
};
&iomuxc {
ipu2 {
pinctrl_ipu2_1: ipu2grp-1 { (Parallel) Image Sensor */
fsl,pins = <
MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC 0x80000000
MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x80000000
MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK 0x80000000
MX6QDL_PAD_EIM_DA9__IPU2_CSI1_DATA00 0x80000000
MX6QDL_PAD_EIM_DA8__IPU2_CSI1_DATA01 0x80000000
MX6QDL_PAD_EIM_DA7__IPU2_CSI1_DATA02 0x80000000
MX6QDL_PAD_EIM_DA6__IPU2_CSI1_DATA03 0x80000000
MX6QDL_PAD_EIM_DA5__IPU2_CSI1_DATA04 0x80000000
MX6QDL_PAD_EIM_DA4__IPU2_CSI1_DATA05 0x80000000
MX6QDL_PAD_EIM_DA3__IPU2_CSI1_DATA06 0x80000000
MX6QDL_PAD_EIM_DA2__IPU2_CSI1_DATA07 0x80000000
MX6QDL_PAD_EIM_DA1__IPU2_CSI1_DATA08 0x80000000
MX6QDL_PAD_EIM_DA0__IPU2_CSI1_DATA09 0x80000000
MX6QDL_PAD_CSI0_DAT16__GPIO6_IO02 0x80000000
MX6QDL_PAD_CSI0_VSYNC__GPIO5_IO21 0x80000000
MX6QDL_PAD_CSI0_DATA_EN__GPIO5_IO20 0x80000000
>;
};
};
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <1>;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};
&i2c1 {
status = "okay";
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1_2>;
ar0331: ar0331@10 {
compatible = "ar0331";
reg = <0x10>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu2_1>;
clock-names = "csi_mclk";
ipu_id = <1>;
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
rst-gpios = <&gpio6 2 1>;
};
};
Hi Zaheer M, what's your sensor's output format and how about the frame length? Please also dump the IPU2_CSI1_SENS_CONF, IPU2_CSI1_SENS_FRM_SIZE, IPU2_CSI1_ACT_FRM_SIZE and IPU2_SMFC_BS registers.
From your IDMAC setting, for each frame, the CSI needs receive 1280*720*2 bytes.
By the way, your data line connection IPU2_CSI1_DATA09 ~ IPU2_CSI1_DATA00 for 10 bits CSI interface is also wrong, you shoudl use IPU2_CSI1_DATA19 ~ IPU2_CSI1_DATA10.
Hi Qiang,
Thanks for responding to the query.
You had mentioned the calculation of 'Frame size' in an earlier post, can you pl. tell me what values would be used for receiving 1280x720 bayer frames.
You have mentioned that we need to use Data-19 to Data-10 for receiving 10-bit data, Can you also mention how to arrive at using which data lines for receiving 10-bit data from the sensor. Is there a mention of it in the data-sheet or the reference manual?
Thanks,
Zaheer.
Yes, the CSI data line MSB information comes from reference manual 37.4.3.2.1 Parallel Interface.
For your setting, the frame size is 1280*720*2, I don't think it is enough for a 10 bits bayer input. If the bayer camera sensor will send 10 bits R, G, B for a pixel, then from CSI side of view, for each pixel, it needs 6 bytes, so the the frame size should be 1280*720*6; and if you use 16 bits generic mode to capture the data, in IDMAC and CSI registers, you can set bpp=16, width = (1280*3) and height = 720; then the CSI can receice a correct frame in (1280*3)*720*2 bytes.
You can seach "MX6QDL_PAD_EIM_D29__IPU2_CSI1_VSYNC" or "MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC" in in file "/arch/arm/boot/dts/imx6q-pinfunc.h"., the select input value had already been defined there.
You can add the IOMUX define into "imx6q.dtsi".
My "imx6q.dtsi" file already has the PAD_PIN configuration, as below. I don't have any sample code for configuration of the input register i.e. "IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT"
&iomuxc {
ipu2 {
pinctrl_ipu2_1: ipu2grp-1 { (Parallel) Image Sensor */
fsl,pins = <
MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC 0x80000000
MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x80000000
MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK 0x80000000
MX6QDL_PAD_EIM_DA9__IPU2_CSI1_DATA00 0x80000000
MX6QDL_PAD_EIM_DA8__IPU2_CSI1_DATA01 0x80000000
MX6QDL_PAD_EIM_DA7__IPU2_CSI1_DATA02 0x80000000
MX6QDL_PAD_EIM_DA6__IPU2_CSI1_DATA03 0x80000000
MX6QDL_PAD_EIM_DA5__IPU2_CSI1_DATA04 0x80000000
MX6QDL_PAD_EIM_DA4__IPU2_CSI1_DATA05 0x80000000
MX6QDL_PAD_EIM_DA3__IPU2_CSI1_DATA06 0x80000000
MX6QDL_PAD_EIM_DA2__IPU2_CSI1_DATA07 0x80000000
MX6QDL_PAD_EIM_DA1__IPU2_CSI1_DATA08 0x80000000
MX6QDL_PAD_EIM_DA0__IPU2_CSI1_DATA09 0x80000000
MX6QDL_PAD_CSI0_DAT16__GPIO6_IO02 0x80000000
MX6QDL_PAD_CSI0_VSYNC__GPIO5_IO21 0x80000000
MX6QDL_PAD_CSI0_DATA_EN__GPIO5_IO20 0x80000000
>;
};
};
You don't need set IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT alone, it was covered in MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC, when the BSP initializing the PIN EIM_DA12 as CSI1_VSYNC, the IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT will be set too.
From the define, we can know the IOMUXC_IPU2_SENS1_VSYNC_SELECT_INPUT register will be set to 0x1.
/*
* The pin function ID is a tuple of
* <mux_reg conf_reg input_reg mux_mode input_val>
*/
#define MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x144 0x458 0x8e4 0x2 0x1
Thanks for the info.
I still don't have the EOF being triggered while capturing the data. Can you guide me which registers i.e. IPU/CSI/IDMAC need to be check to identify the cause of missing EOF.