Hi,
Refer to the L5.10.72_2.2.0-desktop user guide to build and install Ubuntu on 8mplus platform,I tested on the imx8mplus EVK board and found that When Ubuntu is set to automatic login(modity /etc/gdm3/custom.conf , set AutomaticLoginEnable = true) ,In the kernel phase, sdma_transfer_init will be crashed when loading audio driver ,Pls check the log as below:
.............................................................................
.............................................................................
In the system desktop phase,the system can’t play sound, I try to enter "settings" option, both sound option ”output device“ and ”input device“ are shown as nothing(no audio device message) .
Pls help to check the issue,Many thanks!
解決済! 解決策の投稿を見る。
@Zhiming_Liu Good news it work now.Many thanks for your support!
HI,@nxf65025
I tested the four versions in the figure below, only L5.10.9_1.0.0-desktop-alpha did not have the problem. But all customers used GA release of BSP not alpha&beta release of BSP,I really hope to have a patch fix as soon as possible。Many thanks!
hi nxf65025,
when will this bug be fixed?
watching
hello, how about the result?