I'm experiencing an issue where keyframes do not appear (or are not marked correctly) in a gstreamer h264 stream encoded using vpuenc.
There are two reasons for this claim:
GStreamer producer pipeline:
videotestsrc is-live=1 horizontal-speed=1 ! video/x-raw-yuv, width=640, height=480, framerate=30/1, pixel-aspect-ratio=1/1 ! vpuenc codec=6 force-framerate=true seqheader-method=3 bitrate=524288 ! video/x-h264, format=byte-stream ! rtph264pay pt=96 ! udpsink host=192.168.3.120 port=5010
GStreamer consumer pipeline:
udpsrc port=5010 ! application/x-rtp, media=video, clock-rate=90000, encoding-name=H264, payload=96 ! rtph264depay ! h264parse ! filesink location=vpuenc-sample.h264
GStreamer details:
gst-inspect-0.10 version 0.10.35
GStreamer 0.10.35
vpuenc details:
vpuenc versions
plugin: 3.0.7
wrapper: 1.0.35(VPUWRAPPER_ARM_LINUX Build on Dec 20 2013 15:09:05)
vpulib: 5.4.12
firmware: 2.1.9.36350
I do not have this issue when encoding with x264enc instead of vpuenc. Is it possible to get vpuenc to correctly generate/mark periodic keyframes?
Attached are ffprobe frame dumps for recorded streams encoded with vpuenc and x264enc. Notice the key_frame=1 appearing throughout the x264enc dump.
Original Attachment has been moved to: x264enc.h264.frames.txt.zip
Original Attachment has been moved to: vpuenc.h264.frames.txt.zip
解決済! 解決策の投稿を見る。
vpuenc only output I frame based on GOP setting. Default GOP is 15. seems customer need IDR frame based on GOP. Please try attached patch.
BTW, why customer need IDR frame output?
Has anyone found a solution to this yet? I've run into the same issue using vpuenc 3.0.8 on the i.MX6 SABRE SDB.
Martin,
Can you try encoding using unit_tests/mxc_vpu_test.out app and examine the resulting file? This will help us to identify if the problem is at gst level. For example:
./mxc_vpu_test.out -E "-w 640 -h 480 -f 2 -o enc.h264"
For direct comparison, I did this:
gst-launch -v videotestsrc num-buffers=500 ! filesink location=in.yuv
./mxc_vpu_test.out -E "-i in.yuv -w 320 -h 240 -o testout3.h264 -f 2"
Then I used ffprobe -show_frames to look for the key_frame=1 flag. This output also only shows the first frame as a keyframe, so the same problem occurs using those options with mxc_vpu_test.out.
I've written some test code that sets the VPU's "nForceIPicture" flag to 1 every few frames and analyzed that output using the same method; that output does have the key_frame=1 periodically, so the VPU can generate I frames on demand. I just can't find a way in gstreamer to make that happen periodically.
We're using gstreamer for network streaming where the player may pick up the stream already in progress and miss the first frame.
What version of the plugin is this patch for? I can't build either 3.0.7 or 3.0.8 with it, the error is that there is no gop_frm_cnt member of GstVpuEnc.
I'm sorry, I can't get these files to build either - I get this error:
vpuenc.c:538:30: error: 'VpuEncOpenParamSimp' has no member named 'nIsAvcc'
I'm using the source I downloaded from i.MX 6 Series Software and Development Tool Resources as my baseline, that's "L3.0.35_4.1.0_130816_source.gz" with "IMX_MMCODEC_3.0.35_4.1.0_BUNDLE_CODA.gz" installed. Is there something newer I should be using?
Okay, with the patch applied to the latest code I'm seeing the IDR frames and the client is able to pick up the stream. Thank you for your help.
BTW, did you get this error when using x264enc?
No I did not. I am not experiencing an issue with x264enc. My issue is related to vpuenc.