Dear All,
I have newly started working on the iMX6 Dual Lite micro-Q7 board from SECO.
I have built a yocto layer with the following details:
DEFAULTTUNE="cortexa9hf-neon"
MACHINE_FEATURES += " usbhost ethernet wifi bluetooth pci"
When i try to boot the uImage built using the above features, i end up with a kernel panic.
[ 1.006121] Unable to handle kernel NULL pointer dereference at virtual address 00000001
[ 1.014238] pgd = 80004000
[ 1.016953] [00000001] *pgd=00000000
[ 1.020555] Internal error: Oops: 5 [#1] PREEMPT SMP
Detailed bootlog here: iMX6-DL-uQ7-SECO - Pastebin.com
I am able to build the uImage with arm-fsl-linux-gnueabi.
So, the linux sources are working and no issues there.
Kindly have a look and let me know where i am going wrong.
Thanks,
Anup.
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )
Thank you for using Freescale Community.