Issues about MFG tool download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues about MFG tool download

878 Views
tony_l_cai
Contributor III

Hi, all

     The first time I downloaded success, and then I want to start up the board. But it could not work. So I downloaded again,but it stop on the "Load u-boot" ,when I tried again, the same result appeared. Then I checked the DDR, The result is following:

MX6SL opened.

Write to HidMX6x failed.

rom_check_hab: writing cmd to device failed and error code is 997

rom_check_hab() failed.Please make sure board connected and in serial download mode.

What's wrong?

3Q~

Labels (2)
0 Kudos
Reply
1 Reply

703 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

such time to time instability may be caused by

hardware: one can check Chapter 8 Avoiding Board Bring-up Problems

IMX6DQ6SDLHDG and test basic board functionality with SDK

i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply