Issue booting U-boot on i.mx28evk using openocd jtag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue booting U-boot on i.mx28evk using openocd jtag

2,600 Views
B_K_Ankur
Contributor IV

Hello Friends,

I am trying to boot u-boot using Olimex ARM-USB-OCD JTAG on imx28evk. The JTAG gets connected properly but failed to execute the "u-boot.bin" image loaded in RAM.

Below are the steps:

1) Configure the BOOT Switch in NAND boot mode

2) Connect the JTAG with the board

3) Open the Debug Serial Console for i.mx28 under Putty

4) On Linux PC Machine ran the openocd using below command:

    test@test-VirtualBox:~/openocd-0.7.0/tcl$ sudo openocd -f interface/olimex-arm-usb-ocd.cfg -f board/imx28evk.cfg

    Open On-Chip Debugger 0.7.0 (2014-03-17-18:03)

    Licensed under GNU GPL v2

    For bug reports, read

            http://openocd.sourceforge.net/doc/doxygen/bugs.html

    Info : only one transport option; autoselect 'jtag'

    trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst

    adapter_nsrst_delay: 100

    jtag_ntrst_delay: 100

    dcc downloads are enabled

    adapter speed: 9000 kHz

    test_init

    Info : clock speed 6000 kHz

    Info : JTAG tap: imx28.cpu tap/device found: 0x079264f3 (mfg: 0x279, part: 0x7926, ver: 0x0)

    Info : Embedded ICE version 6

    Info : imx28.cpu: hardware has 2 breakpoint/watchpoint units

4) Open the Telnet to JTAG at port 4444. Ran the Init for imx28 and load the image

    test@test-VirtualBox:~/openocd-0.7.0/tcl$ telnet localhost 4444

    Trying 127.0.0.1...

    Connected to localhost.

    Escape character is '^]'.

    Open On-Chip Debugger

    > imx28evk_init                                           

    target state: halted

    target halted in Thumb state due to debug-request, current mode: Supervisor

    cpsr: 0x00000073 pc: 0xfffe6478

    MMU: disabled, D-Cache: disabled, I-Cache: disabled

    > load_image u-boot.bin 0x40000100   

    No working memory available. Specify -work-area-phys to target.

    not enough working area available(requested 24)

    no working area available, falling back to memory writes

    444820 bytes written at address 0x40000100

    downloaded 444820 bytes in 97.281677s (4.465 KiB/s)

  

5) Execute the loaded image:

    > resume 0x40000100

    >

6)  Nothing comes out of Debug Console it remains blank.

Can anyone share their views what I am missing here? I have referred links: https://community.freescale.com/thread/302010 and https://community.freescale.com/thread/309446 but still couldnt able to boot u-boot from RAM.

Additional Info Output at telnet prompt:

> scan_chain

   TapName             Enabled  IdCode     Expected   IrLen IrCap IrMask

-- ------------------- -------- ---------- ---------- ----- ----- ------

0 imx28.cpu              Y     0x079264f3 0x079264f3     4 0x01  0x0f

Thank you in Advance.

Regards,

Ankur

Labels (2)
Tags (3)
0 Kudos
Reply
8 Replies

1,247 Views
Wlodek_D_
Senior Contributor II

Dear Ankur Patel,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

Hello Wlodek_D,

Thank you for pointing out. I am sorry, I missed selecting correct community.

Regards,

Ankur

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

For More Information: The u-boot.sd and u-boot.nand generated via above u-boot.bin (which is failing to load via JTAG) are working fine and tested.

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

Hello Folks,

I am still struggling to run the u-boot on the RAM. Even tried with the pre-compiled u-boot.bin file. Any suggestions are welcome..

Regards,

Ankur

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

Hello Friends,

I found reading Re: Has anyone used an FTDI 2232 based JTAG probe on an IMX28? post that to boot from JTAG, I have to kept boot mode for imx28evk into JTAG by configuring the boot switches to 0 1 1 0. In case if I do then I got error as below

test@test-VirtualBox:~/openocd/openocd-0.7.0/tcl$ sudo openocd -f interface/olimex-arm-usb-ocd.cfg -f board/imx28evk.cfg

Open On-Chip Debugger 0.7.0 (2014-03-17-18:03)

Licensed under GNU GPL v2

For bug reports, read

        http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'jtag'

trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

dcc downloads are enabled

adapter speed: 9000 kHz

3145728

Info : clock speed 6000 kHz

Error: JTAG scan chain interrogation failed: all zeroes

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: imx28.cpu: IR capture error; saw 0x00 not 0x01

Warn : Bypassing JTAG setup events due to errors

Info : Embedded ICE version 0

Error: unknown EmbeddedICE version (comms ctrl: 0x00000000)

Info : imx28.cpu: hardware has 2 breakpoint/watchpoint units

In other boot modes, I can connect successfully with JTAG. Configuring it to NAND boot mode, I got below message:

test@test-VirtualBox:~/openocd/openocd-0.7.0/tcl$ sudo openocd -f interface/olimex-arm-usb-ocd.cfg -f board/imx28evk.cfg

Open On-Chip Debugger 0.7.0 (2014-03-17-18:03)

Licensed under GNU GPL v2

For bug reports, read

        http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'jtag'

trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

dcc downloads are enabled

adapter speed: 9000 kHz

3145728

Info : clock speed 6000 kHz

Info : JTAG tap: imx28.cpu tap/device found: 0x079264f3 (mfg: 0x279, part: 0x7926, ver: 0x0)

Info : Embedded ICE version 6

Info : imx28.cpu: hardware has 2 breakpoint/watchpoint units

My concern is in which mode I have to kept the boot switches to load and boot the u-boot.bin file?

Regards,

Ankur.

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

Hello Friends,

Assuming that Jtag is working in NAND mode, I have followed  Re: Has anyone used an FTDI 2232 based JTAG probe on an IMX28? to load u-boot image step by step mentioned. But I am getting "undefined Instruction" when I do resume 0x40000100.


Could anyone point what is missing?

Regards,

Ankur

0 Kudos
Reply

1,247 Views
B_K_Ankur
Contributor IV

Now using USB boot mode for debugging.

Thanks,

Ankur.

0 Kudos
Reply

1,246 Views
cono
Contributor I

Hi Ankur,

it is no problem to load U-Boot into the DDR of i.MX28. See post Re: Load u-boot with JTAG

Regards,

Christoph

arvero GmbH

0 Kudos
Reply