Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

776 次查看
hrushinale
Contributor III

Hello All,

I want to interface the MSR with i.MX6 Dualite processor. As I search the sample I got the product with external USB interface but I want to interafce it directly to the processor .

Please Suggest me the solutions for the same.

Best Regards,

Hrushi

标记 (1)
0 项奖励
回复
2 回复数

702 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

it depends on MSR model, if it has additional interfaces which could be

used for such purpose. So one can contact vendor or check MSR schematic.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

702 次查看
hrushinale
Contributor III

Hello igorpadykov,

Thanks for your Reply.

can you suggest such MSR Models Part Number and Vendor Names which has such additional interfaces.

Best Regards,

Hrushi

0 项奖励
回复