Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

736件の閲覧回数
hrushinale
Contributor III

Hello All,

I want to interface the MSR with i.MX6 Dualite processor. As I search the sample I got the product with external USB interface but I want to interafce it directly to the processor .

Please Suggest me the solutions for the same.

Best Regards,

Hrushi

タグ(1)
0 件の賞賛
返信
2 返答(返信)

662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

it depends on MSR model, if it has additional interfaces which could be

used for such purpose. So one can contact vendor or check MSR schematic.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

662件の閲覧回数
hrushinale
Contributor III

Hello igorpadykov,

Thanks for your Reply.

can you suggest such MSR Models Part Number and Vendor Names which has such additional interfaces.

Best Regards,

Hrushi

0 件の賞賛
返信