Is there a recommended LPDDR2 for i.MX6DQ PoP package?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a recommended LPDDR2 for i.MX6DQ PoP package?

跳至解决方案
838 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner consider using i.MX6DQ PoP.

They want to know whether there is a Freescale recommended DDR to use i.MX6DQ PoP.

According to the following article, PoP package was designed with Micron, so we guess Micron's LPDDR2 chip is recommended, right?

The mobile package just got smaller | Embedded Beat for Design Engineers

If it is correct, would you let me know the part number of recommended chip?

And would you let me know can we use a LPDDR2 chip provided by other than Micron (Samsun, SK Hynix, etc..) also?

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
563 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

FSL used MT42L128M64D2LL-18WT, other LPDDR2 chips also can be used,

as referenced by link "The mobile...", TechNexion and VISE boards.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
564 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

FSL used MT42L128M64D2LL-18WT, other LPDDR2 chips also can be used,

as referenced by link "The mobile...", TechNexion and VISE boards.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
563 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

I checked MT42L128M64D2LL-18WT ball map, but almost DQ pins of both channels (channel A & B) and DQS & DM pins of channel A are not corresponded with i.MX6DQ PoP ball map.

Was there no problem?

You know byte swapping and bit swapping are not allowed for LPDDR2 by JEDEC standard, so I doubt the misprint of ball map in the datasheet if there was no problem.

Best Regards,

Satoshi Shimoda

0 项奖励
回复