Is there a peripheral library in existence for the i.MX RT1064 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a peripheral library in existence for the i.MX RT1064 ?

532 Views
tamir_michael
Contributor IV

Hello,

I prefer not using the mcuxpresso IDE - is there an alternative peripheral library?

Thanks in advance! 

0 Kudos
Reply
1 Reply

464 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Customers can use the SDK. Select Your device, configuration (host OS, apps, toolchain)

and build the SDK.

Welcome | MCUXpresso SDK Builder 

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply