Hi ,
Can someone please confirm whether the UART0 of M4 core in i.MX8X is shared/used by the SCU for showing debug prints by default?
I came across this in the board.c file of mek board in the SCFW porting kit (L6.1.36_2.1.0_SCFWKIT-1.15.0).
sc_pm_clock_rate_t rate = SC_24MHZ;
static sc_bool_t banner = SC_FALSE;
/* Configure pads */
pad_force_mux(SC_P_ADC_IN2, 1, SC_PAD_CONFIG_NORMAL,
SC_PAD_ISO_OFF);
pad_force_mux(SC_P_ADC_IN3, 1, SC_PAD_CONFIG_NORMAL,
SC_PAD_ISO_OFF);/* Power and enable clock */
pm_force_resource_power_mode_v(SC_R_SC_PID0,
SC_PM_PW_MODE_ON);
pm_force_resource_power_mode_v(SC_R_DBLOGIC,
SC_PM_PW_MODE_ON);
pm_force_resource_power_mode_v(SC_R_DB, SC_PM_PW_MODE_ON);
pm_force_resource_power_mode_v(SC_R_M4_0_UART,
SC_PM_PW_MODE_ON);
(void) pm_set_clock_rate(SC_PT, SC_R_M4_0_UART, SC_PM_CLK_PER,
&rate);
(void) pm_clock_enable(SC_PT, SC_R_M4_0_UART, SC_PM_CLK_PER,
SC_TRUE, SC_FALSE);/* Configure UART */
main_config_debug_uart(LPUART_DEBUG, rate);
From the reference manual(IMX8DQXPRM), I saw that ADC_IN3 pin has only the following muxes and no scu_uart_tx.
Similar mux values are present for ADC_IN2 as well.
The muxing is set for M40_UART0_TX and M40_UART0_RX.
Any help will be deeply appreciated.
解決済! 解決策の投稿を見る。
Hello,
Yes, you are correct, the MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (Uboot/Linux), the second one is used by one of the M4 cores OR the SCFW.
Saludos,
Aldo.
Hello,
Yes, you are correct, the MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (Uboot/Linux), the second one is used by one of the M4 cores OR the SCFW.
Saludos,
Aldo.
Thank You @AldoG for the quick reply.