Is the Micron MT41J128M16KT-125: qualified for i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the Micron MT41J128M16KT-125: qualified for i.mx6

601 Views
RobMauro
Contributor II

Micron is replacing the MT41J128M16JT-125: with the K version which is 1.3V as opposed to the J which is 1.5V.  Will i.MX6 work with the new version?

Labels (1)
0 Kudos
Reply
1 Reply

490 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rob,

yes it is supported also, low limit is 1.283V (DDR3L) as shows

Table 6 "Operating Ranges IMX6DQCEC"   rev.3  2_2014.pdf

i.MX6DQ Datasheet (rev.3, 2/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

0 Kudos
Reply