Hi,
I ma using IMX 6Q SABRE SD. I donot have a SPIDF header on the dev board.
I want to play an ac3 file on HDMI Monitor.
Is the above use case valid ?
If so, how to accomplish the same.
I do not intend to decode the AC3 in software on board.
Solved! Go to Solution.
I tested this sometime ago on a mx6 board and it worked fine:
ac3dec -D hw:1,0 -C test.ac3
-The -C option tells the application to stream AC3 data
I tested this sometime ago on a mx6 board and it worked fine:
ac3dec -D hw:1,0 -C test.ac3
-The -C option tells the application to stream AC3 data
Following link allowed me to do aac playback
https://community.freescale.com/docs/DOC-93745
But I was unable to locate alsa tools under LTIB.
Am I missing something in configuration ?
LTIB distro does not contain alsa-tool package, therefore the only way
is to build it manually from sources. Perhaps it makes sense to port Your
applications to Yocto.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
I am new to embedded systems.
Is there any clear advantage of Yocto over LTIB when it comes to building new packages ?
At least one clear advantage - all further updates will be supported by Freescale
only for Yocto.
~Yuri.
Thanks for the guidance YuriMuhin_ng and FabioEstevam.
I will first setup yocto and then take up the alsa-tools issue.
Subodh,
If you are starting with embedded systems, I would suggest starting with Yocto, as there is a very active community of developers.