Hi All,
We want to know the Wi-Fi Direct Support is there or not in Android 7 Released BSP version 7.1.1_1.0.0?
Can we get Wi-Fi Direct Supported BSP Source?
Interfaces:
As per android, Wi-Fi Direct will support with Normal Wi-Fi Mode only.
If we want to enable wifi direct, wifi should be enabled then only we can use wifi direct.
So is there separate interface is created for Wi-Fi[wlan0] & Wi-Fi Direct[p2p0] or It will work with one interface[wlan0] ?
Thanks in Advance!!!!
Regrads,
Raj.
Hi Aravinth,
I didn't get any attachment in previous mail. Could you please send once?
Regards,
Thanaraj.
The WiFI Direct is enabled by default in n7.1.1 release for BCM4339 WiFi chip. You can find it in Settings->WiFi->More.