Interfacing a transceiver modem through I2S to SAI3 on iMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing a transceiver modem through I2S to SAI3 on iMX6ULL

449件の閲覧回数
kmagi
Contributor III

Hi All,

I am in the process of developing a dummy audio codec driver to interface a transceiver modem which is connected through I2S to SAI3 interface of iMX6ULL.

Here modem is acting as master and CPU slave as the modem CLK line is output.

Could you help me get some reference dummy audio codec driver and the device tree structure for the same?

 

Regards,

Kiran

0 件の賞賛
2 返答(返信)

440件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kmagi

 

for dummy audio codec one can look at below patch

https://patchwork.kernel.org/project/linux-arm-kernel/patch/1462233386-23185-1-git-send-email-festev...

 

Best regards
igor

0 件の賞賛

428件の閲覧回数
kmagi
Contributor III

@igorpadykov 

<correcting subject line from SAI3 to SAI2>

How can I configure/reflect modem parameters,

Master clock – 512 kHz
Sample frequency - 8 kHz , 16 bit samples
0 件の賞賛