1)when the video get the image, and on the PC play it , it have a delay more than 1 second , and I cannot resove it . how to do?
In the imx6, I use the commander:
gst-variable-rtsp-server -u "imxv4l2src device=/dev/video0 ! imxipuvideotransform ! imxvpuenc_h264 bitrate= 10000 ! rtph264pay name=pay0 pt=96"
2) another question , how can I add timestamp in the video?
TKS !
Hello OceanKing,
Try:
gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96"
In order to use VLC or other application as the client, just enter the URL. For timestamp you need to use the Video overlay composition meta (meta:GstVideoOverlayComposition) is supported in i.MX video sinks, convert and compositor. This feature accelerates the text image (such as subtitle, timestamp) blending with video in these plugins with hardware.
Regards
sorry , I describe the problem not correctly.
Hi,I want there is no delay between the camera and the VLC, or human cannot distinguish out obviously there is a latency time .
example:if I move before the camera , 2 seonds later , I can see I moved in the vlc.
how should I do ?