Interfacing IW612 with IMX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing IW612 with IMX8QXP

6,434 Views
jnj
Contributor III

I am currently working on IMX8QXP[L5.15 Kirkstone] and I would like to connect IW612 with IMX8QXP to enable Bluetooth functionality. My goal is to load only the UART Bluetooth firmware, and to achieve this, I am consulting the document titled 'Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS' for validating the Bluetooth interface with the i.MX 8QXP board. Unfortunately, the mentioned file 'UART-FW-LOADER--GPL-src.tgz' is not accessible on the NXP site. Can someone help me in acquiring the release package?

0 Kudos
Reply
39 Replies

3,629 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

Please also note that NXP now advise to use its btnxpuart driver instead of the Linux UART driver + FW loader.

btnxpuart driver can:

- replace Linux UART driver

- automatically download the BT firmware (automatically detect if combo WiFi+BT firmware was downloaded before, and download BT firmware if needed)

- automatically handle deep sleep

 

btnxpuart driver is part of the Linux kernel (CONFIG_BT_NXPUART)

It is available in recent i.MX Linux BSPs (starting 6.1.22 TBC).

 

Please refer to:

 

Regards,

Olivier

 

0 Kudos
Reply

3,626 Views
jnj
Contributor III

Hi @ocourson ,

I am currently working on Linux version 5.15.71_2.2.1, and developments are done with this version. For the design, we are planning to use two LBEE5PL2DL modules, with one as WIFI+BT+BLE and the other one as BT+BLE. Therefore, we are seeking the Linux UART driver + FW loader. Is there any issue with this, or do I need to compulsory change the Linux version to use btnxpuart?

0 Kudos
Reply

3,621 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

It is absolutely not mandatory to switch to btnxpuart.

NXP just advise btnxupart use, because it can simplify customer work (automatic firmware detection and download, automatic deep sleep).

 

Regards,

Olivier

0 Kudos
Reply

3,707 Views
Harvey021
NXP TechSupport
NXP TechSupport

You can access to the link (IW612: 2.4/5 GHz Dual-Band 1x1 Wi-Fi® 6 (802.11ax) + Bluetooth® 5.2 + 802.15.4 Tri-Radio Solution | ...) to download it.

Note: you have to sign in to access authorized secure files.

Regards

Harvey

0 Kudos
Reply

3,704 Views
jnj
Contributor III

Hi @Harvey021 ,

 

Thank you for the quick response. I have checked the mentioned link.But in software section I couldn't see the corresponding file . If I am wrong , please correct me

jnj_0-1707119045678.png

 

Tags (1)
0 Kudos
Reply

3,701 Views
Harvey021
NXP TechSupport
NXP TechSupport

opt for secure Files.

You might have to refer to here (Secure Access Rights | NXP Semiconductors) to get further assistance for checking secure access rights. 

 

Regards

Harvey

0 Kudos
Reply

3,687 Views
jnj
Contributor III

Hi @Harvey021 ,

 

When I opt for the secure files in the software section I am able to see only the below 4 files.

 

jnj_0-1707126181248.png

I Couldn't see the UART-FW-LOADER--GPL-src.tgz as mentioned in the Document.

0 Kudos
Reply

3,676 Views
Harvey021
NXP TechSupport
NXP TechSupport

The reason that you can't see might not have implemented the procedure of authorization.

Please follow up the steps as Request secure access rights

The link () brings help if any question to operate the request. 

And you need to prepare the NDA number from your company during completing the procedure of request as above mentioned.

By the way, the tar package should be included in a compress zip file, similar to: 

Generic_SD-WLAN-UART-BT-IW612-LNX_6_1_55-IMX8-18.99.2.p66.10-18.99.2.p66.10-MM6X18423.P6-GPL

 

Regards

Harvey

 

0 Kudos
Reply

3,654 Views
jnj
Contributor III

Hi @Harvey021 ,

I got a reply "Your registration to NXP Secure Access Rights is complete.".But when I choose iw612 as product and checked secure files , I couldn't see any files similar to Generic_SD-WLAN-UART-BT-IW612-LNX_6_1_55-IMX8-18.99.2.p66.10-18.99.2.p66.10-MM6X18423.P6-GPL.I can see only 10 secure files as below.

 

Screenshot from 2024-02-07 11-57-15.png

jnj_0-1707287521195.png

 

0 Kudos
Reply

3,528 Views
jnj
Contributor III

Hi @Harvey021 ,

Could you please help me to get the previously mentioned files?I have completed the all procedures to get the access to the secure files.

0 Kudos
Reply

3,523 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

We asked internally to grant you access to that software package.

We will come back to you as soon as possible

 

Regards,

Olivier

0 Kudos
Reply

3,495 Views
jnj
Contributor III

Hi @ocourson ,

I can now access more secure files. However, in the release notes, it is mentioned that Linux 6.1.1 is running on i.MX8M Mini. I am currently working on i.MX8QXP with Linux version 5.15.71-2.2.1. Do we have any specific UART driver firmware for this particular platform and Linux version? I have downloaded this Linux_SD-UART-BT-IW612-18.99.2.p19.17-18.99.2.p19.17-MXM6X18398.p9-GPL file .Can I Use the same for IMX8QXP?

0 Kudos
Reply

3,486 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

These SW releases apply to all i.MX6/7/8/9 Linux hosts (kernel 2.6.32 to 6.3.0), so you can use them on IMX8QXP with Linux kernel 5.15.71.

Linux_SD-UART-BT-IW612-18.99.2.p19.17-18.99.2.p19.17-MXM6X18398.p9-GPL is not the latest release.

Don't you have access to below release (or newer) ?

Generic_SD-WLAN-UART-BT-IW612-LNX_6_1_55-IMX8-18.99.2.p66.10-18.99.2.p66.10-MM6X18423.P6-GPL

 

Regards,

Olivier

0 Kudos
Reply

3,482 Views
jnj
Contributor III

Hi @ocourson ,

Thank you for the response. Yes, I have access to the above-mentioned file. To enable Bluetooth functionality, I will  flash the 'uartspi_n61x_v1.bin.se[bluetooth only firmware]' file to the chip over UART using the 'UART-FW-LOADER-350-src.tgz' and the following command:


./fw_loader /dev/ttymxcX 115200 0 /lib/firmware/nxp/<BT_only>.bin


I am seeking confirmation. Could you please confirm whether 'uartspi_n61x_v1.bin.se' is indeed the Bluetooth-only binary file?
 

0 Kudos
Reply

3,477 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

fw_loader is not flashing the firmware, it is copying the firmware to IW612 RAM. It means that this operation needs to be done on each reboot.

- uartspi_n61x_v1.bin.se is the narrowband firmware (handling both bluetooth and 802.15.4), can be loaded over UART, using fw_loader or btnxpuart

- sd_w61x_v1.bin.se is the WiFi firmware, can be loaded over SDIO using moal driver 

- sduart_nw61x_v1.bin.se is the WiFi+Bleutooth+802.15.4 combo firmware, can be loaded ovver SDIO using moal driver

 

Regards,

Olivier

0 Kudos
Reply

3,474 Views
jnj
Contributor III

Hi @ocourson ,

Thank you so much for the support.I have one more query.If I am switching to IW611 can I use the same fw and fwloader ?

0 Kudos
Reply

3,470 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @jnj 

 

Yes, IW612 and IW611 use the same firmware (802.15.4 only working on IW612).

And fw_loader is common to all NXP Wifi/BT chipsets.

 

Regards,

Olivier

0 Kudos
Reply

3,459 Views
jnj
Contributor III

Hi @ocourson ,

Thank you for the confirmation.Let me check and get back to you

0 Kudos
Reply

3,393 Views
jnj
Contributor III

Hi @ocourson ,

I connected IW612 WiFi/BT Module with the IMX8QXP MEK board and run the following command to download the firmware over UART to enable only bluetooth.But it throws a timeout error as below.

Screenshot from 2024-02-19 15-49-31.png

 Do we need to take care of any hardware connections when connecting the IW612 M.2 module with the M.2 connector on the EVK Board?

0 Kudos
Reply

3,302 Views
jnj
Contributor III

Hi @ocourson ,

Could you please help me here?

0 Kudos
Reply