Hi,
I am trying to interface MIPI-DSI lcd panel with Imx6 Dual lite processor. attached LCD data sheet for reference.
In my default device tree LVDS and HDMI display is already configured and added for MIPI-DSI in dtsi as following:
"
mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "mipi_dsi";
interface_pix_fmt = "RGB24";
mode_str ="TRULY-WVGA";
default_bpp = <24>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
&mipi_dsi {
status = "okay";
ipu_id = <0>;
csi_id = <1>;
v_channel = <0>;
lanes = <2>;
pinctrl-names = "default";
lcd_panel = "TRULY-WVGA";
pinctrl-0 = <&pinctrl_mipi_dsi_reset>;
};
"
I have successfully build it and install it. but i am getting following error on debug.
"
mxc_sdc_fb fb@0: get mxcfb of property fail
mxc_sdc_fb: probe of fb@0 failed with error -22
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
"
As error shows issue is in driver probe and register.
Please help to write proper device probe for MIPI-DSI.
Thanks,
Jignesh Patel
Solved! Go to Solution.
Thanks for guidance,
Finally my MIPI DSI driver and mxc_sdc_fb driver probed, now next is LCD integration.
Issue is boorargs, uboot has LVDS interface. After changing mipi_dsi in videoargs, driver is registered.
Thanks,
Jignesh Patel
Thanks for guidance,
Finally my MIPI DSI driver and mxc_sdc_fb driver probed, now next is LCD integration.
Issue is boorargs, uboot has LVDS interface. After changing mipi_dsi in videoargs, driver is registered.
Thanks,
Jignesh Patel
Hi Jignesh,
Can you please share your corrected bootargs/videoargs here?
Because I am also facing similar issue,
[ 0.405405] mxc_mipi_dsi fb@0: failed to read of property dev_id
After adding dev_id = <0>; and disp_id = <0>; both values in mxcfb1: fb@0 and &mipi_dsi both nodes another error is generating as below:
mxc_mipi_dsi fb@0: failed to get platform resource 0
My current dtsi node details:
mxcfb1: fb@0 {
compatible = "fsl,imx6q-mipi-dsi";
disp_dev = "mipi_dsi";
dev_id = <0>; //added new
disp_id = <0>; //added new, disp_id = <1>;
interface_pix_fmt = "RGB24";
lcd_panel = "TRULY-WVGA";
mode_str ="TRULY-WVGA";
default_bpp = <24>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
&mipi_dsi {
compatible = "fsl,imx6q-mipi-dsi";
dev_id = <0>;
disp_id = <1>;
lcd_panel = "TRULY-WVGA";
// disp-power-on-supply = <®_mipi_dsi_pwr_on>;
reset-gpios = <&gpio6 4 GPIO_ACTIVE_LOW>;
reset-delay-us = <50>;
status = "okay";
};
But, I am not sure whether I need to add dev_id and disp_id at both places or not?
Which another configuration in dtsi I am missing for correct LCD interface?
Please share your suggestions.
Do let me know if more information require.
Regards,
Jaymin
It may the issue of compatible driver found by linux. syntax should be compatible = "fsl,mxc_sdc_fb";
in your case uboot args = " setenv bootargs ${bootargs} video=mxcfb0:dev=mipi_dsi; " in your config file.
Thanks,
Jignesh Patel
Hi Jignesh
one can try with nxp bsps (rebuilding all from scratch) as it uses different
names, for example : "dev_id , disp_id", v_channel used for mipi_csi
imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
imx6dl.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor for guiding,
Now I have changed my device tree as given link as below:
mxcfb1:fb@0{
compatible = "fsl,imx6q-mipi-dsi";
disp_dev = "mipi_dsi";
interface_pix_fmt = "RGB24";
lcd_panel = "TRULY-WVGA";
mode_str ="TRULY-WVGA";
default_bpp = <24>;
int_clk = <0>;
lete_init = <0>;
status = "okay";
};
&mipi_dsi {
compatible = "fsl,imx6q-mipi-dsi";
dev_id = <0>;
disp_id = <1>;
lcd_panel = "TRULY-WVGA";
disp-power-on-supply = <®_mipi_dsi_pwr_on>;
reset-gpios = <&gpio5 15 GPIO_ACTIVE_LOW>;
reset-delay-us = <50000>;
status = "okay";
};
But still i am getting error:
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
mxc_mipi_dsi fb@0: failed to read of property dev_id
mxc_mipi_dsi: probe of fb@0 failed with error -22
Error is from mipi_dsi.c file.Why it gives the error of dev_id.
Is any other configuration is required for MIPI-DSI and mxcfb1?
Thanks,
Jignesh Patel
Hi Jignesh
recommended to use nxp linux where these settings work fine
Linux L4.14.78_1.0.0 Documentation
Best regards
igor