If iMX8M with DDR3L design,the platform need to patch bl31.bin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

If iMX8M with DDR3L design,the platform need to patch bl31.bin?

跳至解决方案
1,315 次查看
felixhsu
Contributor III

Hi All

The community had release for LPDDR4 bl31.bin patch, if customer use DDR3L design platform, the platform need to patch bl31.bin or not?

https://community.nxp.com/docs/DOC-340179 

Thanks.

标签 (2)
0 项奖励
回复
1 解答
891 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Generally the Arm trusted firmware BL31 should not depend on memory type.

The patch is intended for DVFS and will work only with same type memories as our EVK.


Look at the following:

imx8mq GA release: DDR initialization in ATF 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
892 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Generally the Arm trusted firmware BL31 should not depend on memory type.

The patch is intended for DVFS and will work only with same type memories as our EVK.


Look at the following:

imx8mq GA release: DDR initialization in ATF 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复