I appear to have a similar problem to a few others however solutions provided are not working for my situation.
Up until a few days ago, I was able to debug my 1050 evkb without fail. I started a new project and the Wire Ack Fault error started to appear. Troubleshooting efforts so far:
I am operating on MCUXpresso version 11.5.1 and SDK 2.11.1.
Board connected to computer via J28:
Stream of events are as follows. Error logs attached.
Any help is greatly appreciated.
已解决! 转到解答。
Thank you for your help. The solution in my case was to do the following:
Marking this solution as solved.
Hi @kwolley ,
Don't worry, it's easy to recover, you just need to do the external memory erase at first in the serial download mode, normally, your issue is caused by the flash is downloaded with the abnormal code, then it will also cause the debug issues.
Follow me now!
1. board enter the serial download mode
Power off the board, SW7:1-OFF,2-ON,3-OFF,4-ON
Power on the board
2. Find another USB cable, connect to J9
3. Use the MCUbootUtility to connect your board, and do the mass erase.
About the MCUbootUtility, you can download it from this link:
https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v3.5.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility
4. After the mass erase finished, then you can power off the board, and change the
SW7:1-OFF,2-ON,3-ON,4-OFF
Then, use the MCUXpresso IDE project try to connect the board again with CMSIS DAP if you don't change the on board debugger, it should be OK.
You can check this picture to check which on board debugger you are using now:
Control Panel\Hardware and Sound\Devices and Printers
Please try it on your side, any updated information, please kindly let me know.
Best Regards,
Kerry
Thank you for getting back to me. The board does not recognize a device is connected.
However it appears in the device manager:
Current board setup:
What am I missing?
Thank you for your help. The solution in my case was to do the following:
Marking this solution as solved.
Hello @kwolley @kerryzhou ,
I have the same problem but with a different EVB (FRDM-KW38). Do you know what steps I need to take for this board?
Any hint/help is much appreciated.
Cheers,
Nader
Hi @ArianRF ,
Any KW38 issues, please create your own new question post in this area:
https://community.nxp.com/t5/Wireless-Connectivity/bd-p/wireless-connectivity
Wish it helps you!
Best Regards,
kerry
Hi @kwolley
So, it works now, right?
That's good, if it is working now, please help to mark the correct answer, just to close this case, any new issues, welcome to create the new question post, thanks.
Best Regards,
Kerry