00000.000 MCUXpresso IDE RedlinkMulti Driver v11.5 (Apr 7 2022 16:04:36 - crt_emu_cm_redlink build 11) ( 0) Reading remote configuration Wc(03). No cache support. 00002.314 Found chip XML file in C:/Users/karaw/Documents/MCUXpressoIDE_11.5.1_7266/workspace/evkbimxrt1050_hello_world/Debug\MIMXRT1052xxxxB.xml ( 5) Remote configuration complete 00002.315 emu ConnectToServer 00002.315 Reconnected to existing LinkServer process. 00002.315 emu ConnectProbeCore 1 0 0 0x8000 00002.493 emu ProbeCore failed 0x5 00002.493 Connecting to probe 1 core 0 (using server started externally) reports: 'Ee(42). Could not connect to core.' 00002.493 Retrying... 00003.003 emu ConnectProbeCore 1 0 0 0x8000 00003.023 emu ProbeCore failed 0x5 00003.539 emu ConnectProbeCore 1 0 0 0x8000 00003.540 emu ProbeCore failed 0x5 00004.045 emu ConnectToServer 00004.046 Reconnected to existing LinkServer process. 00004.046 emu ConnectProbeCore 1 0 0 0x8000 00004.048 emu ScriptLoadRunWithVarsToStringBuffer "(null)" "C:\nxp\MCUXpressoIDE_11.5.1_7266\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.5.1.202204071413\binaries\Scripts\RT1050_connect.scp" 00004.176 ============= SCRIPT: RT1050_connect.scp ============= 00004.176 RT1050 Connect Script 00004.176 DpID = 0BD11477 00004.176 Error: Wire Ack Fault - target connected? 00004.176 Error: Wire Ack Fault - target connected? 00004.176 Disabling MPU 00004.176 Error: Wire Ack Fault - target connected? 00004.176 Error: Wire Ack Fault - target connected? 00004.176 Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM 00004.176 Error: Wire Ack Fault - target connected? 00004.176 Error: Wire Ack Fault - target connected? 00004.177 Error: Wire Ack Fault - target connected? 00004.177 Finished 00004.177 ============= END SCRIPT ============================= 00004.177 emu ProbeFindFirst 00004.178 emu ConnectProbeCore 1 0 0 0x8000 00004.203 emu ProbeCore failed 0x5 Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port (100) Target Connection Failed