IMXRT and RS-485

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT and RS-485

1,080件の閲覧回数
anjalikkrishna
Contributor III

Hi,

 I am using MCUXpresso IDE for programming and debugging the imxrt1050 evk .  My task is to display various data in the GUI based on the serial data received via RS485. Whether RS-485 support is there in the basic SDK for this EVK.

How can I check this?

Thanks & Regards,

Anjali

タグ(3)
0 件の賞賛
返信
2 返答(返信)

745件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anjalik

supported features one can find in attached Release Notes included in software package,

seems this is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

745件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I have internal  update:

"RS-485 can be built with the UART interface. "

Best regards
igor

0 件の賞賛
返信