IMX8mp HDMI EDDC I2C configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mp HDMI EDDC I2C configuration

ソリューションへジャンプ
1,321件の閲覧回数
TerryBarnaby1
Contributor V

We are bringing up a new imx8mp board that we have designed. All is functional except the HDMI interface. It almost works with some monitors.

Basically the issue is that the system can't read the DDC data across the HDMI's I2C bus. The design we have is identical to one we have used on another imx8mp board, but we are using the latest NXP 6.1.55_2.2.0 Yocto Linux system.

Looking at the HDMI I2C signals to the monitor it looks like the SCL to SDA timings are a bit off. SDA is changing very close to the SCL -ve transition and we wonder if this could be the cause.

This I2C bus appears to be driven by a special I2C EDID E-DDC interface in the imx8mp. I can't see any particular settings for this in the DTS.

1. Where is the configuration for this I2C type of device ?

2. Has anyone seen this issue before ?

3. Any ideas ?

0 件の賞賛
返信
1 解決策
1,187件の閲覧回数
TerryBarnaby1
Contributor V

I have found the issue. We are using a micro HDMI connector on this board. We used a Wurth 685119248123 part and went with the pinout defined on that datasheet. This was wrong. They have updated the datasheet to a 0002.000 version.

However the DDC I2C timings do look a little tight to me. I tried increasing the value in the EDDC I2C DDC SDA Hold Register and timings look better to me.

Sorry for the noise.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,188件の閲覧回数
TerryBarnaby1
Contributor V

I have found the issue. We are using a micro HDMI connector on this board. We used a Wurth 685119248123 part and went with the pinout defined on that datasheet. This was wrong. They have updated the datasheet to a 0002.000 version.

However the DDC I2C timings do look a little tight to me. I tried increasing the value in the EDDC I2C DDC SDA Hold Register and timings look better to me.

Sorry for the noise.

0 件の賞賛
返信
1,315件の閲覧回数
TerryBarnaby1
Contributor V

This is what the HDMI I2C lines when trying to read I2C device 0x50 address 0. There is no ack from the monitor.

0 件の賞賛
返信