IMX8QM: Wi-Fi firmware download error while reset the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM: Wi-Fi firmware download error while reset the board

1,106件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

 

Hardware: IMX8QM Custom Board + 88w8987 chipset

Software: Yocto - L 5.10

 

I am facing wifi firmware load error while software reboot and hardware reset, not in on and off the board.

And also I am not handling any reset configuration from device tree.

 

Please find the log and let me know what I missing,

 


mwifiex_sdio mmc2:0001:1: WLAN FW already running! Skip FW dnld
mwifiex_sdio mmc2:0001:1: WLAN FW is active
mwifiex_sdio mmc2:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id = 0xa9, act = 0x0
mwifiex_sdio mmc2:0001:1: num_data_h2c_failure = 0
mwifiex_sdio mmc2:0001:1: num_cmd_h2c_failure = 0
mwifiex_sdio mmc2:0001:1: is_cmd_timedout = 1
mwifiex_sdio mmc2:0001:1: num_tx_timeout = 0
mwifiex_sdio mmc2:0001:1: last_cmd_index = 1
mwifiex_sdio mmc2:0001:1: last_cmd_id: 00 00 a9 00 00 00 00 00 00 00
mwifiex_sdio mmc2:0001:1: last_cmd_act: 00 00 00 00 00 00 00 00 00 00
mwifiex_sdio mmc2:0001:1: last_cmd_resp_index = 0
mwifiex_sdio mmc2:0001:1: last_cmd_resp_id: 00 00 00 00 00 00 00 00 00 00
mwifiex_sdio mmc2:0001:1: last_event_index = 0
mwifiex_sdio mmc2:0001:1: last_event: 00 00 00 00 00 00 00 00 00 00
mwifiex_sdio mmc2:0001:1: data_sent=1 cmd_sent=1
mwifiex_sdio mmc2:0001:1: ps_mode=0 ps_state=0
mwifiex_sdio mmc2:0001:1: info: _mwifiex_fw_dpc: unregister device

 

 

 

Regards,
Vinothkumar Sekar
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,085件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

one can try to reset 88w8987, for example in AzureWave AW-CM358SM (it was used for

testing 88w8987 as described in Table 67. On-board chips and external solutions for Bluetooth and Wi-Fi support   i.MX Linux User’s Guide​ )  it is signal PDn described on p.13 datasheet

https://www.azurewave.com/img/nxp/AW-CM358_DS_DF_C_STD.pdf

 

Best regards
igor

0 件の賞賛
返信

1,072件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you igorpadykov for the reply,

I will try and update you.

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信