Hi,
IMX8QM-MEK + Android 11 Automotive
I am getting following build error with modified kernel defconfig,
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system/etc/vintf/compatibility_matrix.2.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/system_ext/etc/vintf/': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system_ext/etc/vintf/manifest.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/product/etc/vintf/': No such file or directory
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] files are incompatible: Runtime info and framework compatibility matrix are incompatible: No compatible kernel requirement found (kernel FCM version = 5).
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] For kernel requirements at matrix level 5, Missing config CONFIG_SHADOW_CALL_STACK
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] : Success
INCOMPATIBLE
[ 99% 768/771] Installed file list: out/target/product/mek_8q/installed-files-recovery.txt
[ 99% 769/771] Target vendor fs image: out/target/product/mek_8q/vendor.img
ninja: build stopped: subcommand failed.
18:33:51 ninja failed with: exit status 1^[[0;31m#### failed to build some targets (03:06 (mm:ss)) ####^[[00m
已解决! 转到解答。
Thank you @Bio_TICFSL for the reply.
This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.
Thank you @Bio_TICFSL for the reply.
This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.