IMX8QM EVK Booting Bootloader with SD card resetting CPU continuously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QM EVK Booting Bootloader with SD card resetting CPU continuously

4,541 次查看
hiteshviradiya
Contributor III

Dear All,

We are exploring IMX8QM EVK to use in our future product. To get start with it we had purchased IMX8QM EVK.

As a BSP Engineer, I am building Bootloader and preparing SD card to boot with it.

I am following instructions given in "i.MX Linux® User's Guide" section 4.5.13 How to build imx-boot image by using imx-mkimage" for which I managed from here and there all required binaries (ATF, U-boot (u-boot-spl.bin, u-boot-nodtb.bin and fsl-imx8mq-evk.dtb), HDMI and DDR firmwares) mentioned in this section and generated Bootloader flash.bin file

I copied it to SD card using "sudo dd if=flash.bin of=/dev/sdc bs=1k seek=33 conv=fsync" and set bootmodes (using SW801 and SW802) correctly. It has booted from it but it looks like it failed to load 2nd stage bootloader. See below detailed log:

U-Boot SPL 2017.03 (Oct 29 2018 - 18:24:55)
PMIC:  PFUZE100 ID=0x10
start to config phy: p0=3200mts, p1=667mts with 1D2D training
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
config to do 3200 1d training.
Training PASS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
config to do 3200 2d training.
Training PASS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
pstate=1: set dfi clk done done
Training PASS
Load 201711 PIE
Normal Boot
Trying to boot from MMC2
"Synchronous Abort" handler, esr 0x02000000
ELR:     80004364
LR:      910020
x0 : 0000000000915180 x1 : 000000004100d030
x2 : 0000000080004364 x3 : 00000000ff00fff0
x4 : 00000000009151a0 x5 : 00000000009151c0
x6 : 00000000401ffd7f x7 : 0000000000000003
x8 : 000000000000028c x9 : 0000000000000001
x10: 0000000000185bac x11: 00000000401ffa40
x12: 0000000000000259 x13: 000000000000024c
x14: 0000000000185bec x15: 00000000401ffa40
x16: 0000000000008558 x17: 000000000000000c
x18: 0000000000185e40 x19: 0000000000910020
x20: 00000000007f2a88 x21: 0000000000000000
x22: 00000000007f06c3 x23: 0000000000185df0
x24: 00000000007f06ab x25: 00000000007f2000
x26: 00000000deadbeef x27: 0000000000000000
x28: 0000000000000000 x29: 0000000000185d80

Resetting CPU ...

But if I use "imx-boot-imx8mqevk-sd.bin-flash_evk" file present inside L4.9.88_2.0.0_images_MX8MQ.tar.gz it boots up very well.

My Question: What am I missing to generated Bootloader which works like pre-built binaries?

Also I observed that section 4.5.13 mentioned to copy bl31.bin file to imx-mkimage git repo tool but there is no rule to use it in file iMX8M/soc.mak which is called when running "make SOC=iMX8M flash_hdmi_spl_uboot" command.

--

Thanks,

Hitesh

0 项奖励
5 回复数

2,266 次查看
hiteshviradiya
Contributor III

This thread is closed ! All the problems resolved including building ATF firmware from source code. The mistake I was doing was "make PLAT=imx8qm bl31" but my EVK is having imx8mq pltform. Very confusing names imx8qm v/s imx8mq

So after building ATF using "make PLAT=imx8mq bl31" and putting it to generate Bootloader resolves the issue!!

0 项奖励

2,266 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Histesh

The reason may be ddr errors so one can run ddr test and rebuild image using

guidelines in Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx

included in package

i.MX 8M DDR Tool Release 

0 项奖励

2,266 次查看
hiteshviradiya
Contributor III

This is resolved by replacing ATF (ARM Trusted Firmware) binary bl31.bin from https://community.nxp.com/servlet/JiveServlet/download/340179-27-427786/bl31.bin.zip  instead of generating from repo code.

Any idea what I might be missing in generation of ATF firmware from code?

BTW, I have already applied https://community.nxp.com/servlet/JiveServlet/download/340179-27-428410/0001-ATF-support-to-differen... patch

--

Thanks,

Hitesh

0 项奖励

2,266 次查看
hiteshviradiya
Contributor III

I think it is not DDR issue because if I fill bootloader with all 4 DDR firmware bins (lpddr4_pmu_train_*.bin), It passes all the DDR tests and looks for 2nd stage Bootloader. And if I generate flash.bin w/o it, It stuck at DDR test stage boot up.

So 1st stage bootloader generation process is all good (which includes padding of 4 DDR firmware files & concatenating with u-boot-spl.bin)

But SPL fails to find 2nd stage Bootloader (which is u-boot.itb generated by means of mkimage_fit_atf.sh script which internally uses u-boot-nodtb.bin, fsl-imx8mq-evk.dtb and ATF bl31.bin).

So either u-boot.itb generation issue or offset which 1st stage bootloader looks for 2nd stage bootloader issue.

Please provide valuable inputs.

--

Thanks,

Hitesh

0 项奖励

2,266 次查看
hiteshviradiya
Contributor III

Thank you dear for the prompt response!

I will check this but My question is: I am trying this with EVK so doesn't the DDR firmware binaries which is available on NXP are correct (which I used to generate flash.bin)?

I will try your suggested link and revert,

--

Thanks,

Hitesh

0 项奖励