power consumption about imx6 solox?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

power consumption about imx6 solox?

563 Views
zhanghan
Contributor II

          Now I want to design a pad using  imx6 solox based on  the official development board with Peripherals such as wifi, bluetooth, GPS, PCIE, CAMERA.and 10.1 inch LCD .How do I calculate the power consumption to choose the right lithium battery?

Labels (1)
0 Kudos
3 Replies

470 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

one can look at sect.4.1.5 Maximum Supply Currents i.MX6SX Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

and AN5050 i.MX6SX Power Consumption

https://www.nxp.com/docs/en/application-note/AN5050.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

470 Views
zhanghan
Contributor II

Is there a power consumption calculation tool that I can use?  I still need to add the power consumption of the SSD, the power consumption of the wifi module, the power consumption of the Bluetooth module, the power consumption of the LCD liquid crystal, and other peripheral devices.right?

0 Kudos

470 Views
igorpadykov
NXP Employee
NXP Employee

>Is there a power consumption calculation tool that I can use? 

no.

Best regards
igor

0 Kudos