Dear All,
LCD and HDMI are working individually.
How to configure the dual display support in imx8qm - "imx-yocto-L4.14.78_1.0.0_ga" release.
1. LCD - 1080x1920 (MIPI-DSI1)
2. HDMI.
Regards,
Prashanth Kumar K
Dear Joan Xie,
We are checked “fsl-imx8qm-mek.dtsi” file for Dual display, in that Two LVDS/MIPI-DSI Displays are supported, each LVDS/MIPI-DSI is from different Display controller.
In our case both the displays (Native HDMI and MIPI-DSI-1) are from to single Display controller (DPU).
Please share the changes for Dual Display support using single Display controller (DPU).
Best Regards,
Prashanth Kumar K
I haven't imx8 board to test for you , but you can try to use fsl-imx8qm-mek.dtb, which should support dual display.