IMX8MQ USB Wakeup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ USB Wakeup

5,847 Views
Jack19
Contributor I

Hello all,

I am attempting to use USB to wake from a low power mode on an MIMX8MQ6CVAHZAA with i.MX Linux Kernel 5.4. To test, I am using the following procedure with a USB keyboard:

# check that the keyboard device wakeup is enabled
$ cat /sys/bus/usb/devices/1-1/power/wakeup
enabled

# suspend system
$ echo deep > /sys/power/state

I expect the system to resume on a key press, but nothing happens.

I am aware of erratum e11231 from this document applicable to the processor. A related NXP community post (user @RayW8d had a very similar goal) indicates that there is a patch for e11231. However, it does not appear that this patch was made public.

Please advise on how to achieve this wakeup functionality via USB.

Thank you in advance.

0 Kudos
Reply
11 Replies

5,185 Views
ZRay
Contributor I

Hi,

Does this method also work on desktop?
I have the same need on desktop and would like some help.

Thank you.

0 Kudos
Reply

5,161 Views
Jack19
Contributor I
Hi @ZRay,
Can you clarify what you mean by "on desktop"? Is this related to an NXP product?
Thanks
0 Kudos
Reply

5,143 Views
ZRay
Contributor I

Hi @Jack19,

My customer is using i.MX8MQ with nxp-desktop (Kernel version 5.15.32)

They want to resume the system via USB, but it seems that patch is needed.

Thank you.

0 Kudos
Reply

5,807 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Dear Jack,

@Jack19 I already email the patches to you, please have a check.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply

2,989 Views
huangbaokang
Contributor II

Hello, Could you please send this patches to me too?  we need this patch too.

0 Kudos
Reply

2,933 Views
huangbaokang
Contributor II

@Rita_Wang  have any feedback ?

0 Kudos
Reply

4,946 Views
antoluk
Contributor II
Hello, Could you please send this patches to me too?
0 Kudos
Reply

5,719 Views
Roman_Loz
Contributor I

Hi,
I tried this on imx8mp and had the same result (nothing).
Could you please help me too?

0 Kudos
Reply

5,688 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@Roman_Loz I email to you, please have a check.

0 Kudos
Reply

5,685 Views
Roman_Loz
Contributor I

Thank you for your help.
I am trying to wakeup imx8mp (not imx8mq) and the Kernel based on tag lf-6.1.22-2.0.0.
Are there any patches for that?

0 Kudos
Reply

5,643 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @Roman_Loz ,

We do not have this patch for the i.MX8MP, but you can try to refer to the patch for the i.MX8MQ.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply