ubuntu22.04 and 18.04 environment will give error, do not know how to deal with
ERROR: pseudo-native-1.9.0+gitAUTOINC+060058bb29-r0 do_compile: oe_runmake failed
ERROR: pseudo-native-1.9.0+gitAUTOINC+060058bb29-r0 do_compile: ExecutionError('/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304', 1, None, None)
ERROR: Logfile of failure stored in: /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/log.do_compile.3658304
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: Building/installing only 64-bit libpseudo.so for pseudo-native.
| NOTE: If you need to run 32-bit executables, ensure that NO32LIBS is set to 0.
| SQLite header for version 3038005 found in /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr.
| Enabling in-memory database by default.
| NOTE: make -j 24 RPATH=-Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/
| CC="gcc -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/" ./makewrappers "xattr=true"
| ./maketables enums/*.in
| mkdir -p lib/pseudo/lib64
| mkdir -p bin
| enums/debug_type.in: Flags: set for debug_type
| type: debug_type_t (prefix 'PDBG_ENUM')
| extra column: unsigned char symbolic (default '\0')
| extra column: const char * description (default NULL)
| consistency file op pid
| client server db xattrdb
| profile syscall env chroot
| path sql wrapper ipc
| invoke benchmark verbose xattr
|
| enums/exit_status.in: type: exit_status_t (prefix 'PSEUDO_EXIT_ENUM')
| extra column: char * message (default "exit status unknown")
| general fork_failed lock_path lock_held
| lock_failed timeout waitpid socket_create
| socket_fd socket_path socket_unlink socket_bind
| socket_listen listen_fd pseudo_loaded pseudo_prefix
| pseudo_invocation epoll_create epoll_ctl
|
| enums/msg_type.in: type: msg_type_t (prefix 'PSEUDO_MSG_ENUM')
| ping shutdown op ack
| nak fastop
|
| enums/op.in: type: op_t (prefix 'OP_ENUM')
| extra column: int wait (default 0)
| chdir chmod chown chroot
| close creat dup fchmod
| fchown fstat link mkdir
| mknod open rename stat
| unlink symlink exec may-unlink
| did-unlink cancel-unlink get-xattr list-xattr
| remove-xattr set-xattr create-xattr replace-xattr
|
| enums/query_field.in: type: query_field_t (prefix 'PSQF_ENUM')
| access client dev fd
| ftype gid id inode
| mode op order path
| perm program result severity
| stamp tag text type
| uid
|
| enums/query_type.in: type: query_type_t (prefix 'PSQT_ENUM')
| extra column: const char * sql (default "LITTLE BOBBY TABLES")
| exact less greater bitand
| notequal like notlike sqlpat
|
| enums/res.in: type: res_t (prefix 'RESULT_ENUM')
| succeed fail error
|
| enums/sev.in: type: sev_t (prefix 'SEVERITY_ENUM')
| debug info warn error
| critical
|
| Writing datatypes...
| done. Cleaning up.
| gcc -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ -c -o pseudo_tables.o pseudo_tables.c
| Checking for old/new clone mechanics... New clone.
| Considering template: templates/wrapfuncs.h
| Considering template: templates/func_deps
| Considering template: templates/guts
| Considering template: templates/wrapfuncs.c
| Considering template: templates/port_deps
| Considering template: templates/port_wrappers
| Considering template: templates/pseudo_ports
| Considering template: templates/wrapper_table
| common
| ports/common/wrapfuncs.in: .......
| linux
| ports/linux/wrapfuncs.in: ...................................................................
| unix
| ports/unix/wrapfuncs.in: ......................................................................
| unix/syncfs
| ports/unix/syncfs/wrapfuncs.in: .
| uids_generic
| ports/uids_generic/wrapfuncs.in: ........................
| linux/newclone
| ports/linux/newclone/wrapfuncs.in: .
| linux/xattr
| ports/linux/xattr/wrapfuncs.in: ............
| linux/statvfs
| ports/linux/statvfs/wrapfuncs.in: .
| linux/statx
| ports/linux/statx/wrapfuncs.in: .
| Writing functions...
| Warning: lchown from linux overriding unix
| Warning: mknod from linux overriding unix
| Warning: mknodat from linux overriding unix
| Warning: statvfs from linux/statvfs overriding linux
| done. Cleaning up.
| gcc -fno-strict-aliasing -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ -D_GNU_SOURCE -c -o pseudo_wrappers.o pseudo_wrappers.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo_client.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo_ipc.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo_util.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo_db.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudo_server.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudodb.c
| gcc -c -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ pseudolog.c
| pseudo_client.c: In function ‘exec_chroot_scriptcheck’:
| pseudo_client.c:2276:22: warning: assignment discards ‘const’ qualifier from pointer target type [-Wdiscarded-qualifiers]
| 2276 | argv = *argvp;
| | ^
| pseudo_client.c: In function ‘pseudo_exec_path’:
| pseudo_client.c:2468:40: warning: returning ‘int’ from a function with return type ‘const char *’ makes pointer from integer without a cast [-Wint-conversion]
| 2468 | return -1;
| | ^
| pseudo_client.c: In function ‘pseudo_client_op’:
| pseudo_client.c:1863:17: warning: this statement may fall through [-Wimplicit-fallthrough=]
| 1863 | pseudo_client_path(fd, path);
| | ^~~~~~~~~~~~~~~~~~~~~~~~~~~~
| pseudo_client.c:1864:9: note: here
| 1864 | case OP_EXEC: /* fallthrough */
| | ^~~~
| In file included from pseudo_wrappers.c:299:
| pseudo_wrapfuncs.c:8678:49: warning: argument 2 of type ‘const struct timeval *’ declared as a pointer [-Warray-parameter=]
| 8678 | lutimes(const char *path, const struct timeval *tv) {
| | ~~~~~~~~~~~~~~~~~~~~~~^~
| In file included from pseudo_wrappers.c:27:
| /usr/include/x86_64-linux-gnu/sys/time.h:189:62: note: previously declared as an array ‘const struct timeval[2]’
| 189 | extern int lutimes (const char *__file, const struct timeval __tvp[2])
| | ~~~~~~~~~~~~~~~~~~~~~^~~~~~~~
| pseudo_client.c: In function ‘patternlistmatchespath’:
| pseudo_client.c:1476:16: warning: function may return address of local variable [-Wreturn-local-addr]
| 1476 | return foundpath;
| | ^~~~~~~~~
| pseudo_client.c:1442:22: note: declared here
| 1442 | char patternbuf[NAME_MAX];
| | ^~~~~~~~~~
| In file included from pseudo_wrappers.c:299:
| pseudo_wrapfuncs.c:13936:14: warning: argument 1 of type ‘char *’ declared as a pointer [-Warray-parameter=]
| 13936 | tmpnam(char *s) {
| | ~~~~~~^
| In file included from pseudo_wrappers.c:13:
| /usr/include/stdio.h:205:22: note: previously declared as an array ‘char[20]’
| 205 | extern char *tmpnam (char[L_tmpnam]) __THROW __wur;
| | ^~~~~~~~~~~~~~
| In file included from pseudo_wrappers.c:299:
| pseudo_wrapfuncs.c:14665:48: warning: argument 2 of type ‘const struct timeval *’ declared as a pointer [-Warray-parameter=]
| 14665 | utimes(const char *path, const struct timeval *times) {
| | ~~~~~~~~~~~~~~~~~~~~~~^~~~~
| In file included from pseudo_wrappers.c:27:
| /usr/include/x86_64-linux-gnu/sys/time.h:162:61: note: previously declared as an array ‘const struct timeval[2]’
| 162 | extern int utimes (const char *__file, const struct timeval __tvp[2])
| | ~~~~~~~~~~~~~~~~~~~~~^~~~~~~~
| pseudo_client.c: In function ‘pseudo_client_op’:
| cc1: warning: function may return address of local variable [-Wreturn-local-addr]
| pseudo_client.c:1577:22: note: declared here
| 1577 | pseudo_msg_t msg = { .type = PSEUDO_MSG_OP };
| | ^~~
| gcc -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -pipe -std=gnu99 -Wall -W -Wextra -fPIC -D_LARGEFILE64_SOURCE -D_ATFILE_SOURCE -isystem/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -O2 -pipe -DPSEUDO_PREFIX='"/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr"' -DPSEUDO_SUFFIX='""' -DPSEUDO_BINDIR='"bin"' -DPSEUDO_LIBDIR='"lib/pseudo/lib64"' -DPSEUDO_LOCALSTATEDIR='"var/pseudo"' -DPSEUDO_VERSION='"1.9.0"' -DUSE_MEMORY_DB -DPSEUDO_FORCE_ASYNC -DPSEUDO_PASSWD_FALLBACK='NULL' -DPSEUDO_XATTR_SUPPORT -DPSEUDO_EPOLL -O2 -g -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -I/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/include -Wl,--rpath=XORIGIN/../../../sqlite3-native/usr/lib/ -o bin/pseudodb pseudodb.o \
| pseudo_db.o pseudo_tables.o pseudo_util.o pseudo_ipc.o -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -L/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/lyf/work/nxp-desktop/build-desktop/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -lsqlite3 -lpthread -ldl -lpthread
| /home/lyf/work/nxp-desktop/build-desktop/tmp/hosttools/ld: pseudo_db.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: multiple definition of `pseudo_access_t'; pseudodb.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: first defined here
| /home/lyf/work/nxp-desktop/build-desktop/tmp/hosttools/ld: pseudo_util.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: multiple definition of `pseudo_access_t'; pseudodb.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: first defined here
| /home/lyf/work/nxp-desktop/build-desktop/tmp/hosttools/ld: pseudo_ipc.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: multiple definition of `pseudo_access_t'; pseudodb.o:/home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/git/pseudo_ipc.h:37: first defined here
| collect2: error: ld returned 1 exit status
| make: *** [Makefile:113: bin/pseudodb] Error 1
| make: *** Waiting for unfinished jobs....
| ERROR: oe_runmake failed
| WARNING: /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304:238 exit 1 from 'exit 1'
| WARNING: Backtrace (BB generated script):
| #1: bbfatal_log, /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304, line 238
| #2: die, /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304, line 215
| #3: oe_runmake, /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304, line 201
| #4: do_compile, /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304, line 167
| #5: main, /home/lyf/work/nxp-desktop/build-desktop/tmp/work/x86_64-linux/pseudo-native/1.9.0+gitAUTOINC+060058bb29-r0/temp/run.do_compile.3658304, line 251
ERROR: Task (virtual:native:/home/lyf/work/nxp-desktop/sources/meta-nxp-desktop/recipes-devtools/pseudo/pseudo_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 932 tasks of which 883 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/home/lyf/work/nxp-desktop/sources/meta-nxp-desktop/recipes-devtools/pseudo/pseudo_git.bb:do_compile
Summary: There were 2 ERROR messages, returning a non-zero exit code.
https://lists.openembedded.org/g/openembedded-core/topic/patch_pseudo_fix_build_with/78393178
doesn't seem to work either.
I have the same problem, ubuntu22.04, kirkstone-ls-5.15.71-2.2.0.
Has this issue been resolved?
Which desktop version and which build command you use?
Thanks for reply.My desktop version is kirkstone-5.15.71-2.2.0 and the build command is bitbake imx-image-desktop -c populate_sdk
I have exactly the same issue. Did you got it resolved?