Hi,
I want to compile DSP Framework code and generate bin file with Xtensa Xplorer 8.0.13 IDE. According to "XPLORIMX8MPUG_Rev0.pdf":
1) cloning "imx-audio-framework"
2) Registration with MAC_ADDRESS
3) downloading and adding the configuration to Xtensa Xplorer IDE
4) Creating a new project and Importing "imx-audio-framework"
5) adding Linker in build Propertise: "~\imx-audio-framework\dsp_framework\memmap\imx8m"
However, when I execute "build Active", I receive the following error:
**** Incremental Build [星期一, 26 二月 2024 15:40:50] ****
Project: dsp_framework
Configuration: hifi4_mscale_v1_0_2_prod
Build Target: Debug
********************************
"C:\\usr\\xtensa\\XtDevTools\\install\\tools\\RI-2020.4-win32\\XtensaTools\\bin\\xt-xcc" -c -g -O0 -DPLATF_8M -fmessage-length=0 -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/arch\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/arch/libloader/include\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/component/audio\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/include\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/include/audio\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/include/lib\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/plugins/audio_codec\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/plugins/audio_codec/uni_audio\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/plugins/renderer\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/bm\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/freertos\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/qnx\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/threadx\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/xos\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/environment/zephyr\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/aarch64\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx6sx_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx7d_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx7ulp_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8mm_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8mn_m7\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8mp_m7\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8mq_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8qm_m4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8qx_cm4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8ulp_fusionf1\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imx8ulp_m33\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt1160\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt1170\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt500_fusionf1\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt500_m33\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt600_hifi4\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/imxrt600_m33\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/k32l3a6\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/lpc5410x\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/lpc5411x\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/lpc55s69\"" -I "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/rpmsg-lite/lib/include/platform/mcxnx4x\"" -DPROC_hifi4_mscale_v1_0_2_prod -DCONFIG_hifi4_mscale_v1_0_2_prod --xtensa-system=C:/usr/xtensa/XtDevTools/install/builds/RI-2020.4-win32/hifi4_mscale_v1_0_2_prod/config --xtensa-core=hifi4_mscale_v1_0_2_prod --xtensa-params= "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/ipc/rpmsg_platform.c\"" -o "\"C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/bin/hifi4_mscale_v1_0_2_prod/Debug/ipc/rpmsg_platform.o\""
C:/usr/xtensa/Xplorer-8.0.13-workspaces/workspace/dsp_framework/ipc/rpmsg_platform.c:11:34: error: fsl_device_registers.h: No such file or directory
Time taken: 248 ms
Build error encountered... cannot continue further.
Total time taken: 0.923 secs
**** Build Finished [星期一, 26 二月 2024 15:40:51] ****
So, I want to know why this error is reported and how I can fix it.At the same time, my ultimate goal is to use imx8mp's Arm + dsp. Is there more infomation that will allow me to set up a development environment more easyily. Thanks!
解決済! 解決策の投稿を見る。
hi JorgeCas,
Very happy and grateful for your reply.
We previously referred to the i.MX DSP User's Guide document to operate. We just can't find the file fsl_device_registers.h. Can you tell me where exactly this file is?
Hello,
It seems that fsl_device_registers.h is missing on specified route I suggest you add it to see if solves the error.
Is there more information that will allow me to set up a development environment more easily.
The available information related to this is i.MX DSP User's Guide.
Best regards.
hi JorgeCas,
Very happy and grateful for your reply.
We previously referred to the i.MX DSP User's Guide document to operate. We just can't find the file fsl_device_registers.h. Can you tell me where exactly this file is?
Hello panpanjiangjiang,
Since this is licensed software I do not have access to it.
Is it possible to consult it with your FAE or sales-person?
Best regards.