We designed one board based on IMX8MP EVK, we use 2GB LPDDR4, When I use Mscale DDR Tool to Calibration it, I got the following FAILED error.
PMU: Error: Failed write leveling coarse
PMU: ***** Assertion Error - terminating *****
[Result] FAILED
Can you help to check what will cause this?
I use MT53D512M32D2DS-053 WT:D and I will attahce the script file for you to check.
The whole result like follow,
#################################################
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
********Found PMIC PCA9450**********
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
*************************************************************************
Waiting for board configuration from PC-end...
--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122
- MMU and cache setup complete
*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 1500MHz
============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 2048MB
Total density detected on the board is: 2048MB
============================================
MX8M-plus: Cortex-A53 is found
*************************************************************************
============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1500Mhz...
PMU10: **** Start LPDDR4 Training. PMU Firmware Revision 0x1007 ****
PMU10: Setting boot clock divider to 28
PMU10: PHY TOTALS - NUM_DBYTES 4 NUM_NIBBLES 8 NUM_ANIBS 10
PMU10: CSA=0x01, CSB=0x01, TSTAGES=0x131F, HDTOUT=5, MMISC=0 DRAMFreq=3000MT DramType=LPDDR4
PMU10: Pstate0 MRS MR01_A0=0xD4 MR02_A0=0x2D MR03_A0=0x31 MR11_A0=0x66
PMU10: Pstate0 MRS MR12_A0=0x48 MR13_A0=0x00 MR14_A0=0x48 MR22_A0=0x16
PMU10: Pstate0 MRS MR01_B0=0xD4 MR02_B0=0x2D MR03_B0=0x31 MR11_B0=0x66
PMU10: Pstate0 MRS MR12_B0=0x48 MR13_B0=0x00 MR14_B0=0x48 MR22_B0=0x16
PMU5: CA bitmap dump for cs 0
PMU5: CAA0 ffffffff0000000000000007ffffffffffffffffffffffff
PMU5: CAA1 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAA2 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAA3 fffffffe000000000000000fffffffffffffffffffffffff
PMU5: CAA4 ffffffffe000000000000000ffffffffffffffffffffffff
PMU5: CAA5 ffffffff8000000000000007ffffffffffffffffffffffff
PMU5: CA bitmap dump for cs 0
PMU5: CAB0 fffffffff0000000000000007fffffffffffffffffffffff
PMU5: CAB1 ffffffff8000000000000007ffffffffffffffffffffffff
PMU5: CAB2 ffffffff000000000000001fffffffffffffffffffffffff
PMU5: CAB3 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAB4 ffffffffe000000000000000ffffffffffffffffffffffff
PMU5: CAB5 ffffffffc000000000000003ffffffffffffffffffffffff
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
PMU: Error: Failed write leveling coarse
PMU: ***** Assertion Error - terminating *****
[Result] FAILED
Solved! Go to Solution.
Thank you for the help, the issue comes from the hardware, we use one new DDR to resolve this issue.
Thank you for the help, the issue comes from the hardware, we use one new DDR to resolve this issue.
Hi @leavs
Thanks for your quickly reply.
I attached the schematic for LPDDR4 and RPA xlsx sheet.
We use same designe with IMX8MP for LPDDR4, but we use another Micro DDR called MT53D512M32D2DS-053 WT:D, it only have 2GB.
I will try changing PhyVref to 0x11 and back with the result.
I changed PhyVref to 0x11, the same error and result. Is there other option I can try?
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
********Found PMIC PCA9450**********
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
*************************************************************************
Waiting for board configuration from PC-end...
--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122
- MMU and cache setup complete
*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 1500MHz
============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 2048MB
Total density detected on the board is: 2048MB
============================================
MX8M-plus: Cortex-A53 is found
*************************************************************************
============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1500Mhz...
PMU10: **** Start LPDDR4 Training. PMU Firmware Revision 0x1007 ****
PMU10: Setting boot clock divider to 28
PMU10: PHY TOTALS - NUM_DBYTES 4 NUM_NIBBLES 8 NUM_ANIBS 10
PMU10: CSA=0x01, CSB=0x01, TSTAGES=0x131F, HDTOUT=5, MMISC=0 DRAMFreq=3000MT DramType=LPDDR4
PMU10: Pstate0 MRS MR01_A0=0xD4 MR02_A0=0x2D MR03_A0=0x31 MR11_A0=0x66
PMU10: Pstate0 MRS MR12_A0=0x48 MR13_A0=0x00 MR14_A0=0x48 MR22_A0=0x16
PMU10: Pstate0 MRS MR01_B0=0xD4 MR02_B0=0x2D MR03_B0=0x31 MR11_B0=0x66
PMU10: Pstate0 MRS MR12_B0=0x48 MR13_B0=0x00 MR14_B0=0x48 MR22_B0=0x16
PMU5: CA bitmap dump for cs 0
PMU5: CAA0 ffffffff0000000000000007ffffffffffffffffffffffff
PMU5: CAA1 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAA2 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAA3 fffffffe000000000000000fffffffffffffffffffffffff
PMU5: CAA4 ffffffffe000000000000000ffffffffffffffffffffffff
PMU5: CAA5 ffffffff8000000000000007ffffffffffffffffffffffff
PMU5: CA bitmap dump for cs 0
PMU5: CAB0 fffffffff0000000000000007fffffffffffffffffffffff
PMU5: CAB1 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAB2 ffffffff000000000000001fffffffffffffffffffffffff
PMU5: CAB3 ffffffff8000000000000003ffffffffffffffffffffffff
PMU5: CAB4 ffffffffe000000000000000ffffffffffffffffffffffff
PMU5: CAB5 ffffffffc000000000000007ffffffffffffffffffffffff
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
PMU: Error: Failed write leveling coarse
PMU: ***** Assertion Error - terminating *****
[Result] FAILED