Hi NXP Team
Our customer tested CAN bus FD, and the test failed.
They tried setting the data bitrate to 6000k, but it failed.
However, setting the data bitrate to 5000k passed.
Do you have any advice?
Test command: (Test 6000k Fail.)
ip link set can0 up type can bitrate 1000000 dbitrate 6000000 fd on
ip link set can1 up type can bitrate 1000000 dbitrate 6000000 fd on
Test 5000k pass.
解決済! 解決策の投稿を見る。
Hi @kef2
We followed the NXP i.MX8MP DTSI settings, where the CAN clock is set to 40 MHz.
Do you know what the maximum bitrate value could be test pass?
Thanks.
Hi,
I think I wrote already, @40MHz CAN clock, 8Mbps is achievable. The most close speeds are 5 and 8Mbps, no more speeds in between @40Mhz.
Please don't forget as well capabilities of transceiver chips, you are using.
Thanks about your help. 8Mbps pass.
Which version BSP are you using? Are you using NXP evk board or the board you design youself?
About our Image OS is Yocto 3.0-5.4.70.