IMX8MP CAN FD test failed at a data bitrate of 6000k.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP CAN FD test failed at a data bitrate of 6000k.

ソリューションへジャンプ
675件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

Our customer tested CAN bus FD, and the test failed.

They tried setting the data bitrate to 6000k, but it failed.

However, setting the data bitrate to 5000k passed.

Do you have any advice?

Test command:  (Test 6000k Fail.)

ip link set can0 up type can bitrate 1000000 dbitrate 6000000  fd on

ip link set can1 up type can bitrate 1000000 dbitrate 6000000  fd on

charleshuang_0-1723018914421.jpeg

 

Test 5000k pass.

charleshuang_1-1723018978676.jpeg

ラベル(1)
0 件の賞賛
返信
1 解決策
601件の閲覧回数
kef2
Senior Contributor V
Your customer shouldn't ignore "bitrate error 4,7%" message. As you see, he doesn't have such error with 5Mbps.
You can't use every bit rate you wish, but only those, which your CAN clock allows. You didn't specify what is your CAN clock. With 80MHz 8, 5, 4, 3.2, 2.5, 1.6, 1Mbps are possible plus those below 1Mbps. With 40MHz 3.2 is not possible, perhaps 1.6 as well, must check. For 6Mbps I guess you need 30 or 60MHz clock, try calculating it yourself.

元の投稿で解決策を見る

6 返答(返信)
602件の閲覧回数
kef2
Senior Contributor V
Your customer shouldn't ignore "bitrate error 4,7%" message. As you see, he doesn't have such error with 5Mbps.
You can't use every bit rate you wish, but only those, which your CAN clock allows. You didn't specify what is your CAN clock. With 80MHz 8, 5, 4, 3.2, 2.5, 1.6, 1Mbps are possible plus those below 1Mbps. With 40MHz 3.2 is not possible, perhaps 1.6 as well, must check. For 6Mbps I guess you need 30 or 60MHz clock, try calculating it yourself.
573件の閲覧回数
charleshuang
Senior Contributor II

Hi  @kef2 

We followed the NXP i.MX8MP DTSI settings, where the CAN clock is set to 40 MHz.

Do you know what the maximum bitrate value could be test pass?

Thanks.

0 件の賞賛
返信
569件の閲覧回数
kef2
Senior Contributor V

Hi,

I think I wrote already, @40MHz CAN clock, 8Mbps is achievable. The most close speeds are 5 and 8Mbps, no more speeds in between @40Mhz.

Please don't forget as well capabilities of transceiver chips, you are using. 

0 件の賞賛
返信
525件の閲覧回数
charleshuang
Senior Contributor II

@kef2 

Thanks about your help.  8Mbps pass.

0 件の賞賛
返信
636件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? Are you using NXP evk board or the board you design youself?

0 件の賞賛
返信
604件の閲覧回数
charleshuang
Senior Contributor II

@Rita_Wang 

About our Image OS is Yocto 3.0-5.4.70.

0 件の賞賛
返信