IMX8MM evk not able to program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM evk not able to program

1,221件の閲覧回数
santhosh2
Contributor IV

Hello,

Previously i was able to flash the imx8mm evk with new image in emmc,

Observation: The previously loaded image boots properly, But  after changing the switch to flashing mode i am not able to program the new image now. What may be the issue. 

IMG20210804150549.jpg

Regards

Santhosh Kumar S

0 件の賞賛
返信
4 返答(返信)

1,210件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you please share more information, for example how are you trying to flash the eMMC?

I suppose that you're trying to flash Linux, could you share the version as well?

Also, I couldn't see that well the dip switch value from the image you have shared, if possible write the value of the SW1101 & SW1102.

Best regards,
Aldo.

0 件の賞賛
返信

1,196件の閲覧回数
santhosh2
Contributor IV

Hello,

Could you please share more information, for example how are you trying to flash the eMMC?

santhosh: Yes Iam trying to flash into eMMC via serial port (Debug)

I suppose that you're trying to flash Linux, could you share the version as well?

Santhosh: Yes i am trying to flash linux and version is 4.14.78-imx_4.14.78_1.0.0_ga+g94da7bd

I was using below switch position for flashing the image, but from few days i am not able to flash the new image

 12345678910
sw1ONOFFONOFFONONOFFOFFOFFON
           
 12345678910
sw2OFFOFFOFFONOFFONOFFONOFFOFF

 

Please help

 

Regards

Santhosh Kumar S

0 件の賞賛
返信

1,175件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Thank you for sharing more information, everything looks correct, the only thing that I would like you to share more in detail is how are you flashing the image.

For an example on how to flash an i.MX8MM EVK you may refer to the following document:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Flashing-Linux-BSP-using-UUU/ta-p/111067...

Best regards,
Aldo.

0 件の賞賛
返信

1,168件の閲覧回数
santhosh2
Contributor IV

Hello, 

I am using the uuu tool to flash, but the issue i am facing is, its is not detecting the download USB type C port. Normally when you put in program mode it should detect the NXP semiconductor but now the Port is not getting detected,  I am getting the below massage when i do dmesg command in terminal.

What might be the issue

usbdownload.png

 

Regards

Santhosh Kumar S

0 件の賞賛
返信